Block Transfer Error Codes

These are the
Logix5000
block-transfer specific error codes.
Error Code (Hex)
Description
Display In Software
00D0
The scanner did not receive a block-transfer response from the block-transfer module within 3.5 seconds of the request.
Unknown error
00D1
The checksum from the read response did not match the checksum of the data stream.
00D2
The scanner requested either a read or write but the block-transfer module responded with the opposite.
00D3
The scanner requested a length and the block-transfer module responded with a different length.
00D6
The scanner received a response from the block-transfer module indicating the write request failed.
00EA
The scanner was not configured to communicate with the rack that would contain this block-transfer module.
00EB
The logical slot specified is not available for the given rack size.
00EC
There is currently a block-transfer request in progress and a response is required before another request can begin.
00ED
The size of the block-transfer request is not consistent with valid block-transfer size requests.
00EE
The type of block-transfer request is not consistent with the expected BT_READ or BT_WRITE.
00EF
The scanner was unable to find an available slot in the block-transfer table to accommodate the block-transfer request.
00F0
The scanner received a request to reset the remote I/O channels while there were outstanding block-transfers.
00F3
Queues for remote block-transfers are full.
00F5
No communication channels are configured for the requested rack or slot.
00F6
No communication channels are configured for remote I/O.
00F7
The block-transfer timeout, set in the instruction, timed out before completion.
00F8
Error in block-transfer protocol - unsolicited block-transfer.
00F9
Block-transfer data was lost due to a bad communication channel.
00FA
The block-transfer module requested a different length than the associated block-transfer instruction.
00FB
The checksum of the block-transfer read data was wrong.
00FC
There was an invalid transfer of block-transfer write data between the adapter and the block-transfer module.
00FD
The size of the block-transfer plus the size of the index in the block-transfer data table was greater than the size of the block-transfer data table file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal