Power Tab 
    Use this tab to enter the reverse power and reverse var settings.
Parameters
Reverse kW
Setpoint
This value establishes the generator reverse kW setpoint at which the CGCM recognizes a reverse power condition and starts timing to trip, based on the reverse kW fault delay setting. Valid values range from 1.00 to 100.00 % of Rated VA; the default value is 5.00 % of Rated VA.
Fault Delay
This value establishes the time to annunciate and, if configured, to trip the fault output relay once the generator reverse kW setpoint has been exceeded. Valid values range from .10 to 300.00 seconds; the default value is 5.00 seconds.
Reverse kVAR
Setpoint
This value establishes the generator reverse kVar setpoint at which the CGCM recognizes a reverse kVar (loss of excitation) condition and starts timing to trip, based on the reverse kVar fault delay setting. Valid values range from 1.00 to 100.00 % of Rated VA; the default value is 10.00 % of Rated VA.
Fault Delay
This value establishes the time to annunciate and, if configured, to trip the fault output relay once the generator reverse kVar setpoint has been exceeded. Valid values range from .10 to 300.00 seconds; the default value is 20.00 seconds.
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback