Frequency Tab 
    Use this tab to enter overfrequency and underfrequency settings.
Parameters
Over-Frequency
Setpoint
This value establishes the generator overfrequency setpoint at which the CGCM recognizes an overfrequency condition and starts timing to trip, based on the overfrequency time delay. Valid values range from 30.00 to 70.00 Hz; the default value is 60.50 Hz.
Delay
This value establishes the time to annunciate and, if configured, to trip the fault output relay once the generator overfrequency setpoint has been exceeded. Valid values range from .10 to 300.00 seconds; the default value is 1.00 second.
Under-Frequency
Setpoint
This value establishes the generator underfrequency setpoint at which the CGCM recognizes an underfrequency condition and starts timing to trip, based on the underfrequency time delay. Valid values range from 30.00 to 70.00 Hz; the default value is 59.00 Hz.
Delay
This value establishes the time to annunciate and, if configured, to trip the fault output relay once the generator underfrequency setpoint has been exceeded. Valid values range from .10 to 300.00 seconds; the default value is 1.00 second.
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback