instruction

instruction
A mnemonic and data address defining an operation to be performed by the controller. A rung in a program consists of a set of input and output instructions. The input instructions are evaluated by the controller as being True or False. In turn, the controller sets the output instructions to True or False.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal