TransitionalInstruction

This is a transitional instruction. Follow these steps when using it:
  • In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
  • In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal