Time Browser dialog box for relative time

Use the
Time Browser
dialog box to set a relative time (a duration) for a tag using the relative time data types: TIME32, TIME, and LTIME. You can set relative time durations as large as 31 days. To set a duration in nanoseconds, use the LTIME data type.
To set the duration
  1. Enter values in the interval boxes to set up your interval.
  2. In the
    Hour:Minute:Second
    box, select the hours, minutes, or seconds and enter a value, or use the up and down arrows to adjust the value.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal