Use bitwise operators

Bitwise operators manipulate the bits within a value based on two values.
The following provides an overview of the bitwise operators.
For
Use this operator
Optimal data type
bitwise AND
&, AND
DINT
bitwise OR
OR
DINT
bitwise exclusive OR
XOR
DINT
bitwise complement
NOT
DINT
This is an example.
Use this format
Example
For this situation
Use
value1 operator value2
If input1, input2, and result1 are DINT tags and your specification says: "Calculate the bitwise result of input1 and input2. Store the result in result1."
result1 := input1 AND input2;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal