Structured Text Components: Comments

To make your structured text easier to interpret, add comments to it.
  • Comments let you use plain language to describe how your structured text works.
  • Comments do not affect the execution of the structured text.
To add comments to your structured text:
To add a comment
Use one of these formats
on a single line
//comment
(*comment*)
/*comment*/
at the end of a line of structured text
within a line of structured text
(*comment*)
/*comment*/
that spans more than one line
(*start of comment. . .end of comment*)
/*start of comment. . .end of comment*/
For example:
Format
Example
//comment
At the beginning of a line
//Check conveyor belt direction
IF conveyor_direction THEN...
At the end of a line
ELSE //If conveyor isn’t moving, set alarm light
light := 1;
END_IF;
(*comment*)
Sugar.Inlet[:=]1;(*open the inlet*)
IF Sugar.Low (*low level LS*)& Sugar.High (*high level LS*)THEN...
(*Controls the speed of the recirculation pump. The speed depends on the temperature in the tank.*)
IF tank.temp > 200 THEN...
/*comment*/
Sugar.Inlet:=0;/*close the inlet*/
IF bar_code=65 /*A*/ THEN...
/*Gets the number of elements in the Inventory array and stores the value in the Inventory_Items tag*/
SIZE(Inventory,0,Inventory_Items);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal