REPEAT_UNTIL

Use the REPEAT_UNTIL loop to continue performing an action until conditions are true.
Operands
REPEAT
<statement>;
Structured Text
Operand
Type
Format
Enter
bool_
expression
BOOL
Tag expression
BOOL tag or expression that evaluates to a BOOL value
(BOOL expression)
IMPORTANT:
Do not iterate within the loop too many times in a single scan.
The controller does not execute other statements in the routine until it completes the loop.
A major fault occurs when completing the loop takes longer than the watchdog timer for the task.
Consider using a different construct, such as IF_THEN.
Description
The syntax is:
Repeat_Until syntax
The following diagrams show how a REPEAT_UNTIL loop executes and how an EXIT statement leaves the loop early.
While the bool_expression is false, the controller executes only the statements within the REPEAT_UNTIL loop.
RSL5K_REPEAT…UNTIL execution
To stop the loop before the conditions are false, use an EXIT statement.
RSL5K_RSL5K_REPEAT…UNTIL exit
Affects Math Status Flags
No
Fault Conditions
A major fault will occur if
Fault type
Fault code
The construct loops too long
6
1
Example 1
If performing the following,
Enter this structured text
The REPEAT_UNTIL loop executes the statements in the construct and then determines if the conditions are true before executing the statements again. This differs from the WHILE_DO loop because the WHILE_DO The WHILE_DO loop evaluates its conditions first.
If the conditions are true, the controller then executes the statements within the loop. The statements in a REPEAT_UNTIL loop are always executed at least once. The statements in a WHILE_DO loop might never be executed.
pos := -1;
REPEAT
pos := pos + 2;
UNTIL ((pos = 101) OR (structarray[pos].value = targetvalue))
end_repeat;
Example 2
If performing the following,
Enter this structured text
Move ASCII characters from a SINT array into a string tag. (In a SINT array, each element holds one character.) Stop when you reach the carriage return.
Initialize Element_number to 0.
Count the number of elements in SINT_array (array that contains the ASCII characters) and store the result in SINT_array_size (DINT tag).
Set String_tag[element_number] = the character at SINT_array[element_number].
Add 1 to element_number. This lets the controller check the next character in
SINT_array.
Set the Length member of String_tag = element_number. (This records the number of characters in String_tag so far.)
If element_number = SINT_array_size, then stop. (You are at the end of the array and it does not contain a carriage return.)
If the character at SINT_array[element_number] = 13 (decimal value of the carriage return), then stop.
element_number := 0;
SIZE(SINT_array, 0, SINT_array_size);
Repeat
String_tag.DATA[element_number] := SINT_array[element_number];
element_number := element_number + 1;
String_tag.LEN := element_number;
If element_number = SINT_array_size then
exit;
end_if;
Until SINT_array[element_number] = 13
end_repeat;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal