Using Output Limiting (PID)

Set an output limit (percentage of output) on the control output. When the instruction detects that the output has reached a limit, it sets an alarm bit and prevents the output from exceeding either the lower or upper limit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal