Select/Limit Instructions

The Select/Limit instructions include these instructions:
Available Instructions
Ladder Diagram
This instruction is not available in Ladder Diagram.
Function Block and Structured Text
If you want to
Use this instruction
Select one of as many as six inputs.
ESEL
Limit an analog input between two values.
HLL
Select one of eight inputs.
MUX
Limit the amount of change of a signal over time.
RLIM
Select one of two inputs.
SEL
Select between the input value and the negative of the input value.
SNEG
Select real inputs to be summed.
SSUM
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal