Program Conversion Error (PCE)
    The Program Conversion Error (PCE) instruction is generated by the translation tool. The translation tool inserts a PCE instruction within the appropriate ladder rung to help you identify possible errors with a conversion. 
When a file has finished importing, the bottom of the screen displays the results. Double-click on the errors in the results window to locate the PCE messages that the translation tool inserted. To complete the conversion process, you will want to locate, analyze, and fix any discrepancies using the PCE instructions.
An example of a PCE instruction follows:
*** Generated by Translation Tool: Source and destination types may differ *** ; N: PCE(120, PCE011) COP(I1_008, N23[0], 4);
PCE Messages
Below is a list of all of the messages that are generated with a PCE instruction. The text is appended to the rung comments that have the PCE instruction. The message text begins with asterisks(*) and the words "Generated by Translation Tool", and ends with asterisks. 
| ID | Text | Accepted values | 
| 101 | The address references a counter's Update Accum (UA) bit field. This is not supported in  Logix Designersoftware. | Each time a reference to a counter's UA field is encountered ( SLConly). | 
| 102 | The address references a counter's Overflow(OV) or Underflow(UN) field. This has been translated but the translation needs to be validated. | Each time a reference to a counter's OV or UN field is encountered | 
| 103 | Warning: Status files do not exist in  Logix Designersoftware. GSV instructions are used in Logix Designersoftware to obtain controller information where applicable. This translation must be validated. | Each time a reference to the S file is encountered. | 
| 105 | The address references an indirect file number. It was not translated. | Each time an address reference with an indirect file number is encountered. | 
| 107 | The address reference may have an incorrect index. The translation needs to be validated. | Each time suitable index into the array could not be determined. | 
| 108 | The BTR, BTW or MSG instruction has been translated. However, the translation needs to be validated. These instructions have many parameters that cannot be directly translated and require review. | Each time a BTR, BTW or MSG instruction is translated. | 
| 109 | PLC-5and SLCs use 0.01 second and 1 second timebases. Logix Designersoftware uses a 0.001 second time base. The address references ab Accumulator (ACC) field. The translation needs to be validated. | Each time a reference to a ACC field was encountered | 
| 110 | PLC-5and SLCs use 0.01 second and 1 second timebases. Logix Designersoftware uses a 0.001 second time base. The address references a Preset (PRE) field. The translation needs to be validated. | Each time a reference to a PRE field was encountered. | 
| 113 | Follow the <FBC or DDT> instruction with MOV and FAL instruction on parallel branches to ensure the correct bits are being operated on. | Each FBC and DDT instruction. | 
| 114 | Although the PID instruction has been translated, the PID instruction has many parameters that do not translate directly to  Logix Designersoftware. The translation must be verified. | Each time a PID instruction is translated. | 
| 115 | 16-bit parameters have been extended to 32-bit. Ensure bit manipulation is correct. | Each time BSL, BSR, BTD instruction is translated. | 
| 116 | The structure of FOR/NXT/BRK statements has changed in the Logix architecture. In the  PLC-5processor, the FOR and NXT instruction enclosed a section of code that was to be iterated multiple times, while the BRK instruction allowed a way to break out of the repeating code. In the RSLogix architecture, the FOR instruction calls a given routine a specific number of times, so a NXT instruction is not needed. The BRK instruction works in a similar fashion as in the PLC-5processor. Because this architecture change is significant, you will probably have to consider restructuring your logic. | Each time FOR/NXT/BRK instructions are encountered. | 
| 117 | AGA instruction not supported. | Each time a AGA instruction is found. | 
| 119 | CIR/COR not supported. | Each time a CIR or CIO instruction is found. | 
| 120 | Source and destination types differ | When source and destination types differ in a COP instruction. | 
| 121 | DFA instruction not supported | Each time a DFA instruction is found. | 
| 122 | ERI/ERO instruction not supported. | Each time a ERI or ERO instruction is found. | 
| 123 | IDI/IDO instruction not supported. | Each time a IDI or IDO instruction is found. | 
| 124 | IIN/IOT instruction not supported. | Each time a IIN or IOT instruction is found. | 
| 128 | SFC routines aren't translated. | Each time a SFR or EOT instruction is found. | 
| 129 | Online edit instructions are not supported. | Each time a SDS, SIZ or SRZ instruction is found. | 
| 130 | User Interrupt instructions not supported. | Each time a UID, UIE or UIF instruction is found. | 
| 131 | DDV instruction not supported. | Each time a DDV instruction is found. | 
| 132 | High Speed Counter instructions not supported. | Each time a HSC/HSD/HSE/ SL or RHC/RAC/TDF instruction is found. | 
| 133 | I/O Interrupt Enable/Disable instructions not supported. | Each time a IID or IIE instruction is found. | 
| 134 | IIM/IOM instruction not supported. | Each time a IIM or IOM instruction is found. | 
| 135 | INT instruction not supported. | Each time a INT instruction is found. | 
| 136 | REF instruction not supported. | Each time a REF instruction (in  SLC) is found. | 
| 137 | RPI instruction not supported. | Each time a RPI instruction is found. | 
| 138 | Selectable Timed Interrupt instructions not supported. | Each time a STD/STE or STS instruction is found. | 
| 139 | SUS instruction not supported. | Each time a SUS instruction is found. | 
| 141 | RMP instruction not supported. | Each time a RMP instruction is found. | 
| 142 | RPC instruction not supported. | Each time a RPC instruction is found. | 
| 143 | SVC instruction not supported. | Each time a SVC instruction is found. | 
| 144 | SWP instruction not supported. | Each time a SWP instruction is found. | 
| 145 | SQC instruction not supported. | Each time a SQC instruction is found. | 
| 146 | INV instruction not supported. | Each time a INV instruction is found. | 
| 147 | DCD/ENC instruction not supported. | Each time a DCD or ENC instruction is found. | 
| 148 | The CEM, DEM, or EEM instruction has been translated. However, the translation needs to be validated. These instructions have many parameters that cannot be directly translated and require review. | Each time a CEM, DEM or EEM instruction is found. | 
| 149 | Modbus messaging is not supported in  Logix Designersoftware. | If MSG instruction is configured for Modbus. | 
| 150 | MSG instruction and associated MESSAGE tag need to be manually verified. | Each time a MSG instruction is found. | 
| 151 | Warning: Status files do not exist in  Logix Designersoftware. However this status file value is handled through the StatusFile routine. | S file type indexes that can be directly translated to functionality in  Logix Designersoftware. | 
| 152 | Logix Designersoftware has a different fault handling mechanism then the PLC-5/ SLC. This fault routine will not be called. | Start of identified legacy processor fault routine. | 
| 153 | This PII/DII routine is not used by  Logix Designersoftware. | Start of identified legacy processor PII/DII routine. | 
Provide Feedback