Jump to External Routine (JXR)
This information applies to the
SoftLogix
5800 controller only.The JXR instruction executes an external routine.
Available Languages
Ladder Diagram

Function Block
This instruction is not available for function block.
Structured Text
This instruction is not available for structured text.
Operands
Ladder Diagram
Operand | Type | Format | Description |
External routine name | ROUTINE | Name | External routine to execute |
External routine control | EXT_ROUTINE_CONTROL | Tag | Control structure |
Parameter | BOOL SINT INT DINT REAL structure | Immediate Tag Array tag | Data from this routine that you want to copy to a variable in the external routine Parameters are optional. Enter multiple parameters, if needed. You can have as many as 10 parameters. |
Return parameter | BOOL SINT INT DINT REAL | Tag | Tag in this routine to which you want to copy a result of the external routine The return parameter is optional. You can have only one return parameter |
EXT_ROUTINE_CONTROL Structure
Mnemonic | Data Type | Description | Implementation | ||||||||
ErrorCode | SINT | If an error occurs, this value identifies the error. Valid values are from 0-255. | There are no predefined error codes. The developer of the external routine must provide the error codes. | ||||||||
NumParams | SINT | This value indicates the number of parameters associated with this instruction. | Display only - this information is derived from the instruction entry. | ||||||||
ParameterDefs | EXT_ROUTINE_ PARAMETERS[10] | This array contains definitions of the parameters to pass to the external routine. The instruction can pass as many as 10 parameters. | Display only - this information is derived from the instruction entry. | ||||||||
ReturnParamDef | EXT_ROUTIN_ PARAMETERS | This value contains definitions of the return parameter from the external routine. There is only one return parameter. | Display only - this information is derived from the instruction entry. | ||||||||
EN | BOOL | When set, the enable bit indicates that the JXR instruction is enabled. | The external routine sets this bit. | ||||||||
ReturnsValue | BOOL | If set, this bit indicates that a return parameter was entered for the instruction. If cleared, this bit indicates that no return parameter was entered for the instruction. | Display only - this information is derived from the instruction entry. | ||||||||
DN | BOOL | The done bit is set when the external routine has executed once to completion. | The external routine sets this bit. | ||||||||
ER | BOOL | The error bit is set if an error occurs. The instruction stops executing until the program clears the error bit. | The external routine sets this bit. | ||||||||
FirstScan | BOOL | This bit identifies whether this is the first scan after switching the controller to Run mode. Use FirstScan to initialize the external routine, if needed. | The controller sets this bit to reflect scan status. | ||||||||
EnableOut | BOOL | Enable output. | The external routine sets this bit. | ||||||||
EnableIn | BOOL | Enable input. | The controller sets this bit to reflect rung-condition-in. The instruction executes regardless of rung condition. The developer of the external routine should monitor this status and act accordingly. | ||||||||
User1 | BOOL | These bits are available for the user. The controller does not initialize these bits. | Either the external routine or the user program can set these bits. | ||||||||
User0 | BOOL | ||||||||||
ScanType1 | BOOL | These bits identify the current scan type:
| The controller sets these bits to reflect scan status. | ||||||||
ScanType0 | BOOL |
Description
Use the Jump to External Routine (JXR) instruction to call the external routine from a ladder routine in your project. The JXR instruction supports multiple parameters so you can pass values between the ladder routine and the external routine.
The JXR instruction is similar to the Jump to Subroutine ( JSR) instruction. The JXR instruction initiates the execution of the specified external routine:
- The external routine executes one time.
- After the external routine executes, logic execution returns to the routine that contains the JXR instruction.
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if | Fault Type | Fault Code: |
An exception occurs in the external routine DLL. The DLL could not be loaded. The entry point was not found in the DLL. | 4 | 88 |
Execution
The JXR can be synchronous or asynchronous depending on the implementation of the DLL. The code in the DLL also determines how to respond to scan status, rung-condition-in status, and rung-condition-out status.
For more information on using the JXR instruction and creating external routines, see thehttps://literature.rockwellautomation.com/idc/groups/literature/documents/um/1789-um002_-en-p.pdf.
Provide Feedback