Switch Program Control to Operator
    The PIDE instruction can be controlled by either a user program or an operator interface. You can change the control mode at any time. Program and
Operator control use the same ProgOper output. When ProgOper is set, control is Program; when ProgOper is cleared, control is Operator.
The following diagram shows how the PIDE instruction changes between Program control and Operator control.

For more information on program and operator control, refer to Program/Operator Control.
Provide Feedback