IMC Function Block Tuning Procedure
    Follow these steps to configure the tuner.
- Put the CV into Manual mode.
- Set the AtuneStart parameter.The tuner starts collecting PV and CV data for noise calculation.
- After collecting 60 samples (60*DeltaT) period, the tuner adds StepSize to the CV.After successfully collecting the PV data as a result of the CV step change, the CV assumes its value before the step change and the AtuneStatus, GainTuned, TCTuned, DTTuned, and RespTCTuned parameters are updated.
- Set the AtuneUseModel parameter to copy the tuned parameters to the model parameters.The function block then resets the AtuneUseModel parameter.After a successful AutoTuneDone, the Atune parameter is set to one (1). Tuning completed successfully.
Provide Feedback