Process Mix Proof Valve (PVLVMP)
This information applies to the CompactLogix 5380P and ControlLogix 5580P controllers.
The Process Mix Proof Valve (PVLVMP) instruction controls and monitors feedback from a mix-proof valve in various modes and states, monitoring for fault conditions. This instruction supports mix-proof valves with or without additional connections for cleaning (CIP, clean-in-place) or steaming (SIP, sanitize in place).
Use the PVLVMP instruction to:
- Operate a mix-proof valve with these positions:
- Closed
- Opened
- CIP/SIP leakage cavity (optional)
- Operate a mix-proof valve with these positions, which can pulse the seat being cleaned, or lifted opened and closed, to provide enhanced cleaning. (As the seat is popped open and closed, the flow velocity across the seat is increased compared to the fully open seat position.) Pulse times are configurable.
- Lift upper seat (optional)
- Lift lower seat (optional)
- CIP/SIP upper seat (optional)
- CIP/SIP lower seat (optional)eve
- Operate using a state model that makes sure that valve seats are sequenced properly to avoid cross-contamination.
- Provide six outputs and six inputs. The outputs in each valve state (including intermediate states) are configurable for on and off states. The inputs that verify each valve state are configurable for their required on, required off, and don't care states. Provides feedback checking to make sure that the valve reaches each position, including intermediate positions before moving to the next position. The time for feedback inputs to confirm each state is configurable.
- Display graphic symbols for mix-proof valves in 2-D layouts and 3-D (isometric) layouts for ease in building valve array and routing manifold displays.
- Allow maintenance personnel to take the valve out of service. Note that this capability is not a substitute for hard lockout/tagout (LOTO) procedures.
- Provide inputs for Interlock conditions to drive the valve to the closed state.
- Monitor for I/O communication faults, and close the valve and raise an alarm on a fault.
- Provide an available status for Program command source logic so automation code can determine whether a valve can be controlled.
- Provide a valve virtualization capability. When the mix-proof valve is set to virtual, outputs are left de-energized, and the instruction behaves as if a fully functioning valve were providing feedback.
- Operate from Hand, Maintenance, Override, External, Program, and Operator command sources.
- Provide a maintenance command to toggle a locator or beacon output.
Available Languages
Ladder Diagram

Function Block Diagram

Structured Text
PVLVMP(PVLVMPTag, BusObj);
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand | Type | Format | Description |
---|---|---|---|
PlantPAx Control | P_DISCRETE_MIX_PROOF | tag | Data structure required for proper operation of instruction. |
BusObj | BUS_OBJ | tag | Bus component. |
P_DISCRETE_MIX_PROOF Structure
Public members are standard, visible tag members that are programmatically accessible. Private, hidden members are used in HMI faceplates and are not programmatically accessible. Private members are listed in separate tables after public members.
Public Input Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
EnableIn | BOOL | Not Visible | Not Required | Input | Enable Input - System Defined Parameter Default is true. |
Inp_InitializeReq | BOOL | Not Visible | Not Required | Input | 1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request when reinitialization is needed. The instruction clears this operand automatically. Default is true. |
Inp_OwnerCmd | DINT | Not Visible | Not Required | Input | Owner device command (bitmapped): All bits off = None, .10 = Operator Lock, .11 = Operator Unlock, .12 = Program Lock, .13 = Program Unlock, .14 = Acquire Maintenance, .15 = Release Maintenance, .16 = Acquire External, .17 = Release External, .29 = Echo. Default is 0. |
Inp_OpenLSData | BOOL | Visible | Not Required | Input | Valve open limit switch: 1 = Confirmed opened. Default is false. |
Inp_ClosedLSData | BOOL | Visible | Not Required | Input | Valve closed limit switch: 1 = Confirmed fully closed. Default is false. |
Inp_LowerSeatLSData | BOOL | Visible | Not Required | Input | Valve lower seat lift limit switch: 1 = Confirmed lower seat lifted. Default is false. |
Inp_UpperSeatLSData | BOOL | Visible | Not Required | Input | Valve upper seat lift limit switch: 1 = Confirmed upper seat lifted. Default is false. |
Inp_CavityInletLSData | BOOL | Visible | Not Required | Input | Valve cavity inlet limit switch: 1 = Confirmed cavity inlet opened. Default is false. |
Inp_CavityOutletLSData | BOOL | Visible | Not Required | Input | Valve cavity outlet limit switch: 1 = Confirmed cavity output closed. Default is false. |
Inp_IOFault | BOOL | Visible | Not Required | Input | 1 = I/O communication is faulted, 0 = I/O communication is OK. Default is false. |
Inp_OpenIntlkOK | BOOL | Visible | Not Required | Input | 1 = Open interlocks OK, valve can open, 0 = Interlocks not OK, close valve if target/actual state is opened. Default is true. |
Inp_OpenNBIntlkOK | BOOL | Visible | Not Required | Input | 1 = Open non-bypassable interlocks OK, valve can open, 0 = Interlocks not OK, close valve if target/actual state is open. Default is true. |
Inp_OpenIntlkAvailable | BOOL | Visible | Not Required | Input | 1 = Open interlock availability is OK, show Sts_OpenIntlkAvailable if device is ready except for open interlocks. Default is false. |
Inp_LowerSeatIntlkOK | BOOL | Visible | Not Required | Input | 1 = Lower seat interlocks OK, valve can lift or clean lower seat, 0 = Interlocks not OK, close valve if target/actual state has lower seat lifted. Default is true. |
Inp_LowerSeatNBIntlkOK | BOOL | Visible | Not Required | Input | 1 = Lower seat non-bypassable interlocks OK, valve can lift or clean lower seat, 0 = Interlocks not OK, close valve if target/actual state has lower seat lifted. Default is true. |
Inp_LowerSeatIntlkAvailable | BOOL | Visible | Not Required | Input | 1 = Lower seat interlock availability is OK, show Sts_LowerSeatIntlkAvailable if device is ready except for lower seat interlocks. Default is false. |
Inp_UpperSeatIntlkOK | BOOL | Visible | Not Required | Input | 1 = Upper seat interlocks OK, valve can lift or clean upper seat, 0 = Interlocks not OK, close valve if target/actual state has upper seat lifted. Default is true. |
Inp_UpperSeatNBIntlkOK | BOOL | Visible | Not Required | Input | 1 = Upper seat non-bypassable interlocks OK, valve can lift or clean upper seat, 0 = Interlocks not OK, close valve if target/actual state has upper seat lifted. Default is true. |
Inp_UpperSeatIntlkAvailable | BOOL | Visible | Not Required | Input | 1 = Upper seat interlock availability is OK, show Sts_UpperSeatIntlkAvailable if device is ready except for upper seat interlocks. Default is false. |
Inp_CavityIntlkOK | BOOL | Not Visible | Not Required | Input | 1 = Cavity interlocks OK, valve can clean cavity or seat, 0 = Interlocks not OK, close valve if target/actual state has cleaning via cavity. Default is true. |
Inp_CavityNBIntlkOK | BOOL | Not Visible | Not Required | Input | 1 = Cavity non-bypassable interlocks OK, valve can clean cavity or seat, 0 = Interlocks not OK, close valve if target/actual state has cleaning via cavity. Default is true. |
Inp_CavityIntlkAvailable | BOOL | Not Visible | Not Required | Input | 1 = Cavity interlock availability is OK, show Sts_CavityIntlkAvailable if device is ready except for cavity interlocks. Default is false. |
Inp_IntlkTripInh | BOOL | Visible | Not Required | Input | 1 = Inhibit reporting of Sts_IntlkTrip and interlock trip alarm. Default is false. |
Inp_RdyReset | BOOL | Not Visible | Not Required | Input | 1 = Related object, reset by this object, is ready to be reset. Default is false. |
Inp_Hand | BOOL | Not Visible | Not Required | Input | 1 = Acquire Hand command source (typically hardwired local), 0 = Release Hand. Default is false. |
Inp_Ovrd | BOOL | Not Visible | Not Required | Input | 1 = Acquire Override command source (higher priority program logic), 0 = Release Override. Default is false. |
Inp_OvrdCmd | SINT | Not Visible | Not Required | Input | Override device command: 0 = None, 1 = Close, 2 = Open, 3 = Lift lower seat, 4 = Lift upper seat, 5 = Clean cavity, 6 = Clean lower seat, 7 = Clean upper seat. Default is 0. |
Inp_ExtInh | BOOL | Not Visible | Not Required | Input | 1 = Inhibit External command source acquisition, 0 = Allow External acquisition. Default is false. |
Inp_HornInh | BOOL | Not Visible | Not Required | Input | 1 = Inhibit audible alert, 0 = Allow audible alert. Default is false. |
Inp_Reset | BOOL | Not Visible | Not Required | Input | 1 = Reset shed latches and cleared alarms. Default is false. |
Cfg_AllowDisable | BOOL | Not Visible | Not Required | Input | 1 = Allow Maintenance to disable alarms. Default is true. |
Cfg_AllowShelve | BOOL | Not Visible | Not Required | Input | 1 = Allow Operator to shelve alarms. Default is true. |
Cfg_HasLiftLower | BOOL | Not Visible | Not Required | Input | 1 = Valve supports lift lower seat state. Default is false. |
Cfg_HasLiftUpper | BOOL | Not Visible | Not Required | Input | 1 = Valve supports lift upper seat state. Default is false. |
Cfg_HasCleanCavity | BOOL | Not Visible | Not Required | Input | 1 = Valve supports clean cavity state. Default is false. |
Cfg_HasCleanLower | BOOL | Not Visible | Not Required | Input | 1 = Valve supports clean lower seat state. Default is false. |
Cfg_HasCleanUpper | BOOL | Not Visible | Not Required | Input | 1 = Valve supports clean upper seat state. Default is false. |
Cfg_bOutStateSt0 | SINT | Not Visible | Not Required | Input | Outputs to valve in De-energized state (state 0). Default is 2#0000_0000. |
Cfg_bOutStateSt1 | SINT | Not Visible | Not Required | Input | Outputs to valve in Closed state (state 1). Default is 2#0000_0001. |
Cfg_bOutStateSt2 | SINT | Not Visible | Not Required | Input | Outputs to valve in Close cavity outlet state (state 2). Default is 2#0010_0000. |
Cfg_bOutStateSt3 | SINT | Not Visible | Not Required | Input | Outputs to valve in Open state (state 3). Default is 2#0010_0010. |
Cfg_bOutStateSt4 | SINT | Not Visible | Not Required | Input | Outputs to valve in Lift lower seat state (state 4). Default is 2#0000_0100. |
Cfg_bOutStateSt5 | SINT | Not Visible | Not Required | Input | Outputs to valve in Lift upper seat state (state 5). Default is 2#0000_1000. |
Cfg_bOutStateSt6 | SINT | Not Visible | Not Required | Input | Outputs to valve in Clean cavity state (state 6). Default is 2#0001_0000. |
Cfg_bOutStateSt7 | SINT | Not Visible | Not Required | Input | Outputs to valve in Lift lower seat for cleaning state (state 7). Default is 2#0001_0100. |
Cfg_bOutStateSt8 | SINT | Not Visible | Not Required | Input | Outputs to valve in Clean lower seat state (state 8). Default is 2#0011_0100. |
Cfg_bOutStateSt9 | SINT | Not Visible | Not Required | Input | Outputs to valve in Lift upper seat for cleaning state (state 9). Default is 2#0001_1000. |
Cfg_bOutStateSt10 | SINT | Not Visible | Not Required | Input | Outputs to valve in Clean upper seat state (state 10). Default is 2#0011_1000. |
Cfg_bFdbkStateSt0 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in De-energized state (state 0). Default is 2#0000_0000. |
Cfg_bFdbkStateSt1 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Closed state (state 1). Default is 2#0000_0001. |
Cfg_bFdbkStateSt2 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Close cavity outlet state (state 2). Default is 2#0010_0000. |
Cfg_bFdbkStateSt3 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Open state (state 3). Default is 2#0010_0010. |
Cfg_bFdbkStateSt4 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Lift lower seat state (state 4). Default is 2#0000_0100. |
Cfg_bFdbkStateSt5 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Lift upper seat state (state 5). Default is 2#0000_1000. |
Cfg_bFdbkStateSt6 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Clean cavity state (state 6). Default is 2#0001_0000. |
Cfg_bFdbkStateSt7 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Lift lower seat for cleaning state (state 7). Default is 2#0001_0100. |
Cfg_bFdbkStateSt8 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Clean lower seat state (state 8). Default is 2#0011_0100. |
Cfg_bFdbkStateSt9 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Lift upper seat for cleaning state (state 9). Default is 2#0001_1000. |
Cfg_bFdbkStateSt10 | SINT | Not Visible | Not Required | Input | Feedback input states when valve is in Clean upper seat state (state 10). Default is 2#0011_1000. |
Cfg_bFdbkReqdSt0 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in De-energized state (state 0). Default is 2#0000_1111. |
Cfg_bFdbkReqdSt1 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Closed state (state 1). Default is 2#0000_1111. |
Cfg_bFdbkReqdSt2 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Close cavity outlet state (state 2). Default is 2#0000_1111. |
Cfg_bFdbkReqdSt3 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Open state (state 3). Default is 2#0000_1111. |
Cfg_bFdbkReqdSt4 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Lift lower seat state (state 4). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt5 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Lift upper seat state (state 5). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt6 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Clean cavity state (state 6). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt7 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Lift lower seat for cleaning state (state 7). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt8 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Clean lower seat state (state 8). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt9 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Lift upper seat for cleaning state (state 9). Default is 2#0000_0000. |
Cfg_bFdbkReqdSt10 | SINT | Not Visible | Not Required | Input | Feedback inputs required (checked) to verify valve is in Clean upper seat state (state 10). Default is 2#0000_0000. |
Cfg_FdbkTimeSt0 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached De-energized state (state 0) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt1 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Closed state (state 1) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt2 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Close cavity outlet state (state 2) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt3 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Opened state (state 3) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt4 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Lift lower seat state (state 4) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt5 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Lift upper seat state (state 5) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt6 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Clean cavity state (state 6) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt7 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Lift lower seat for cleaning state (state 7) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt8 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Clean lower seat state (state 8) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt9 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Lift upper seat for cleaning state (state 9) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_FdbkTimeSt10 | REAL | Not Visible | Not Required | Input | Time feedbacks must match required pattern to confirm valve has reached Clean upper seat state (state 10) (seconds). Valid = 0.0 to 60.0. Default is 1.0. |
Cfg_PulseLiftLower | BOOL | Not Visible | Not Required | Input | 1 = Pulse seat lift output when lifting lower seat, 0 = Do not pulse, lift seat continuously. Default is false. |
Cfg_PulseLiftUpper | BOOL | Not Visible | Not Required | Input | 1 = Pulse seat lift output when lifting upper seat, 0 = Do not pulse, lift seat continuously. Default is false. |
Cfg_PulseCleanLower | BOOL | Not Visible | Not Required | Input | 1 = Pulse seat lift output when cleaning lower seat, 0 = Do not pulse, clean continuously. Default is false. |
Cfg_PulseCleanUpper | BOOL | Not Visible | Not Required | Input | 1 = Pulse seat lift output when cleaning upper seat, 0 = Do not pulse, clean continuously. Default is false. |
Cfg_HasOpenIntlkObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object is connected to Inp_OpenIntlkOK, Inp_OpenNBIntlkOK inputs, enable navigation. Default is false. |
Cfg_HasLowerSeatIntlkObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object is connected to Inp_LowerSeatIntlkOK, Inp_LowerSeatNBIntlkOK inputs, enable navigation. Default is false. |
Cfg_HasUpperSeatIntlkObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object is connected to Inp_UpperSeatIntlkOK, Inp_UpperSeatNBIntlkOK inputs, enable navigation. Default is false. |
Cfg_HasCavityIntlkObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object is connected to Inp_CavityIntlkOK, Inp_CavityNBIntlkOK inputs, enable navigation. Default is false. |
Cfg_HasStatsObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI a PVLVS object is monitoring this valve, enable navigation. Default is false. |
Cfg_HasMoreObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object with more information is available, enable navigation. Default is false. |
Cfg_OperClosePrio | BOOL | Not Visible | Not Required | Input | 1 = OCmd_Close is accepted any time, 0 = OCmd_Close is accepted only when Operator command source is selected. Default is false. |
Cfg_ExtClosePrio | BOOL | Not Visible | Not Required | Input | 1 = XCmd_Close is accepted any time, 0 = XCmd_Close is accepted only when External command source is selected. Default is false. |
Cfg_OCmdResets | BOOL | Not Visible | Not Required | Input | 1 = A new Operator state command resets fault, 0 = A reset command is required to clear fault. Default is false. |
Cfg_XCmdResets | BOOL | Not Visible | Not Required | Input | 1 = A new External state command resets fault, 0 = A reset command is required to clear fault. Default is false. |
Cfg_OvrdPermIntlk | BOOL | Not Visible | Not Required | Input | 1 = Override ignores bypassable permissives and interlocks, 0 = Override uses all permissives and interlocks. Default is false. |
Cfg_ShedOnFail | BOOL | Not Visible | Not Required | Input | 1 = Close valve and alarm on position fail, 0 = Alarm only. Default is true. |
Cfg_ShedOnIOFault | BOOL | Not Visible | Not Required | Input | 1 = Close valve and alarm on I/O fault, 0 = Alarm only. Default is true. |
Cfg_HasOper | BOOL | Not Visible | Not Required | Input | 1 = Operator (unlocked) command source exists, can be selected. Default is true. |
Cfg_HasOperLocked | BOOL | Not Visible | Not Required | Input | 1 = Operator Locked command source exists, can be selected. Default is true. |
Cfg_HasProg | BOOL | Not Visible | Not Required | Input | 1 = Program (unlocked) command source exists, can be selected. Default is true. |
Cfg_HasProgLocked | BOOL | Not Visible | Not Required | Input | 1 = Program Locked command source exists, can be selected. Default is true. |
Cfg_HasExt | BOOL | Not Visible | Not Required | Input | 1 = External command source exists, can be selected. Default is false. |
Cfg_HasMaint | BOOL | Not Visible | Not Required | Input | 1 = Maintenance command source exists, can be selected. Default is true. |
Cfg_HasMaintOoS | BOOL | Not Visible | Not Required | Input | 1 = Maintenance Out of Service exists, can be selected. Default is true. |
Cfg_OvrdOverLock | BOOL | Not Visible | Not Required | Input | 1 = Override supersedes Program/Operator Locked, 0 = Don't supersede Program/Operator Locked. Default is true. |
Cfg_ExtOverLock | BOOL | Not Visible | Not Required | Input | 1 = External supersedes Program/Operator Locked, 0 = Don't supersede Program/Operator Locked. Default is false. |
Cfg_ProgPwrUp | BOOL | Not Visible | Not Required | Input | 1 = Power up to Program command source, 0 = Power up to Operator command source. Default is false. |
Cfg_ProgNormal | BOOL | Not Visible | Not Required | Input | Normal command source: 1 = Program, 0 = Operator. Default is false. |
Cfg_PCmdPriority | BOOL | Not Visible | Not Required | Input | Command priority: 1 = Program commands win, 0 = Operator commands win. Default is false. |
Cfg_PCmdProgAsLevel | BOOL | Not Visible | Not Required | Input | 1 = Program/Operator selection follows PCmd_Prog as level (1 for Program, 0 for Operator), 0 = PCmd_Prog is used as edge to select Program, PCmd_Oper selects Operator. Default is false. |
Cfg_PCmdLockAsLevel | BOOL | Not Visible | Not Required | Input | 1 = Program lock selection follows PCmd_Lock as level (1 for locked, 0 for unlocked), 0 = PCmd_Lock is used as edge to select Program Locked, PCmd_Unlock selects Program (unlocked). Default is false. |
Cfg_ExtAcqAsLevel | BOOL | Not Visible | Not Required | Input | 1 = External selection follows XCmd_Acq as level (1 to acquire External, 0 to release External), 0 = XCmd_Acq is used as edge to acquire External, XCmd_Rel is used to release External. Default is false. |
Cfg_OpenPulseTime | REAL | Not Visible | Not Required | Input | Time to lift seat when pulsing for cleaning (seconds). Valid = 0.0 to 2147483.0, 0.0 = do not pulse. Default is 10.0. |
Cfg_ClosePulseTime | REAL | Not Visible | Not Required | Input | Time to close seat when pulsing for cleaning (seconds). Valid = 0.0 to 2147483.0, 0.0 = do not pulse. Default is 5.0. |
Cfg_StartHornTime | REAL | Not Visible | Not Required | Input | Time to sound audible on command to move from the closed position (seconds). Valid = 0.0 to 1000.0, 0.0 = Disabled. Default is 0.0. |
Cfg_FailTime | REAL | Not Visible | Not Required | Input | Time to receive state feedback before declaring failure (seconds). Valid = 0.0 to 2147483.0. Default is 3.0. |
Cfg_CnfrmReqd | SINT | Not Visible | Not Required | Input | Operator command confirmation or e-signature type required: 0 = None, 1 = Command confirmation required, 2 = Performer e-signature required, 3 = Performer and approver e-signature required. Default is 0. |
PSet_Owner | DINT | Not Visible | Not Required | Input | Program ownership request: Non-zero Owner ID = acquire, 0 = release. Default is 0. |
PCmd_Virtual | BOOL | Not Visible | Not Required | Input | Program Command to select Virtual (simulated) device operation. The instruction clears this operand automatically. Default is false. |
PCmd_Physical | BOOL | Not Visible | Not Required | Input | Program Command to select Physical device operation (not simulated). The instruction clears this operand automatically. Default is false. |
PCmd_Close | BOOL | Not Visible | Not Required | Input | Program Command to close valve. The instruction clears this operand automatically. Default is false. |
PCmd_Open | BOOL | Not Visible | Not Required | Input | Program Command to cpen valve. The instruction clears this operand automatically. Default is false. |
PCmd_LiftLower | BOOL | Not Visible | Not Required | Input | Program Command to lift lower seat. The instruction clears this operand automatically. Default is false. |
PCmd_LiftUpper | BOOL | Not Visible | Not Required | Input | Program Command to lift upper seat. The instruction clears this operand automatically. Default is false. |
PCmd_CleanCavity | BOOL | Not Visible | Not Required | Input | Program Command to clean valve leakage cavity. The instruction clears this operand automatically. Default is false. |
PCmd_CleanLower | BOOL | Not Visible | Not Required | Input | Program Command to clean lower seat. The instruction clears this operand automatically. Default is false. |
PCmd_CleanUpper | BOOL | Not Visible | Not Required | Input | Program Command to clean upper seat. The instruction clears this operand automatically. Default is false. |
PCmd_Reset | BOOL | Not Visible | Not Required | Input | Program Command to reset shed latches and returned-to-normal latched alarms. The instruction clears this operand automatically. Default is false. |
PCmd_Prog | BOOL | Not Visible | Not Required | Input | Program Command to select Program command source. The instruction clears this operand automatically if Cfg_PCmdProgAsLevel = 0. Default is false. |
PCmd_Oper | BOOL | Not Visible | Not Required | Input | Program Command to select Operator command source. The instruction clears this operand automatically. Default is false. |
PCmd_Lock | BOOL | Not Visible | Not Required | Input | Program Command to lock Program command source and disallow Operator. The instruction clears this operand automatically if Cfg_PCmdLockAsLevel = 0. Default is false. |
PCmd_Unlock | BOOL | Not Visible | Not Required | Input | Program Command to unlock Program command source and allow Operator to acquire. The instruction clears this operand automatically. Default is false. |
PCmd_Normal | BOOL | Not Visible | Not Required | Input | Program Command to select normal command source (Operator or Program). The instruction clears this operand automatically. Default is false. |
XCmd_Close | BOOL | Not Visible | Not Required | Input | External Command to close valve. The instruction clears this operand automatically. Default is false. |
XCmd_Open | BOOL | Not Visible | Not Required | Input | External Command to cpen valve. The instruction clears this operand automatically. Default is false. |
XCmd_LiftLower | BOOL | Not Visible | Not Required | Input | External Command to lift lower seat. The instruction clears this operand automatically. Default is false. |
XCmd_LiftUpper | BOOL | Not Visible | Not Required | Input | External Command to lift upper seat. The instruction clears this operand automatically. Default is false. |
XCmd_CleanCavity | BOOL | Not Visible | Not Required | Input | External Command to clean valve leakage cavity. The instruction clears this operand automatically. Default is false. |
XCmd_CleanLower | BOOL | Not Visible | Not Required | Input | External Command to clean lower seat. The instruction clears this operand automatically. Default is false. |
XCmd_CleanUpper | BOOL | Not Visible | Not Required | Input | External Command to clean upper seat. The instruction clears this operand automatically. Default is false. |
XCmd_Acq | BOOL | Not Visible | Not Required | Input | External Command to acquire command source. The instruction clears this operand automatically if Cfg_ExtAcqAsLevel = 0. Default is false. |
XCmd_Rel | BOOL | Not Visible | Not Required | Input | External Command to release command source, accepted if Cfg_ExtAcqAsLevel = 0. The instruction clears this operand automatically. Default is false. |
XCmd_Reset | BOOL | Not Visible | Not Required | Input | External Command to reset shed latches and returned-to-normal latched alarms. The instruction clears this operand automatically. Default is false. |
XCmd_ResetAckAll | BOOL | Not Visible | Not Required | Input | External Command to acknowledge all alarms and reset latched alarms and shed conditions. The instruction clears this operand automatically. Default is false. |
Public Output Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
EnableOut | BOOL | Not Visible | Not Required | Output | Enable Output - System Defined Parameter |
Out_OpenData | BOOL | Visible | Not Required | Output | Output to open valve: 1 = Open. |
Out_CloseData | BOOL | Visible | Not Required | Output | Output to close valve: 1 = Close. |
Out_LiftLowerData | BOOL | Visible | Not Required | Output | Output to lift lower valve seat: 1 = Lift. |
Out_LiftUpperData | BOOL | Visible | Not Required | Output | Output to lift upper valve seat: 1 = Lift. |
Out_CavityInletData | BOOL | Visible | Not Required | Output | Output to open leakage cavity cleaning inlet: 1 = Open. |
Out_CavityOutletData | BOOL | Visible | Not Required | Output | Output to close leakage cavity drain/cleaning outlet: 1 = Close. |
Out_LocatorData | BOOL | Not Visible | Not Required | Output | Output to valve locator lamp/beacon: 1 = Illuminated. |
Out_HornData | BOOL | Not Visible | Not Required | Output | Output to sound horn prior to commanded state change. |
Out_Reset | BOOL | Not Visible | Not Required | Output | 1 = Reset command has been received and accepted. |
Out_OwnerSts | DINT | Not Visible | Not Required | Output | Status of command source, owner command handshake and ready status (bitmapped): All bits off = None, .10 = Operator Lock, .11 = Operator Unlock, .12 = Program Lock, .13 = Program Unlock, .14 = Acquire Maintenance, .15 = Release Maintenance, .16 = Acquire External, .17 = Release External, .18 = Has Maintenance, .19 = External Override Lock, .20 = Has External, .21 = Has Operator, .22 = Has Operator Locked, .23 = Has Program, .24 = Has Program Locked, .29 = Echo, .30 = Not Ready. |
Sts_Initialized | BOOL | Not Visible | Not Required | Output | 1 = Instruction is initialized. 0 = Use Inp_InitializeReq to reinitialize. |
Sts_Closed | BOOL | Visible | Not Required | Output | 1 = Valve closed position achieved. |
Sts_Opened | BOOL | Visible | Not Required | Output | 1 = Valve opened position achieved. |
Sts_LiftLower | BOOL | Visible | Not Required | Output | 1 = Lift valve lower seat position achieved. |
Sts_LiftUpper | BOOL | Visible | Not Required | Output | 1 = Lift valve upper seat position achieved. |
Sts_CleanCavity | BOOL | Not Visible | Not Required | Output | 1 = Clean valve leakage cavity position achieved. |
Sts_CleanLower | BOOL | Not Visible | Not Required | Output | 1 = Clean valve lower seat position achieved. |
Sts_CleanUpper | BOOL | Not Visible | Not Required | Output | 1 = Clean valve upper seat position achieved. |
Sts_Moving | BOOL | Visible | Not Required | Output | 1 = Valve not yet confirmed in commanded position. |
Sts_Pulsing | BOOL | Visible | Not Required | Output | 1 = Pulsing valve seat for cleaning. |
Sts_Locator | BOOL | Not Visible | Not Required | Output | 1 = Locator/beacon for identifying valve is active. |
Sts_Horn | BOOL | Not Visible | Not Required | Output | 1 = Sounding horn prior to commanded state change. |
Sts_Physical | BOOL | Not Visible | Not Required | Output | 1 = The instruction is available to control the physical valve, 0 = Instruction is not controlling the physical valve, outputs are holding the valve closed. |
Sts_Virtual | BOOL | Not Visible | Not Required | Output | 1 = The instruction is available to control a virtual model of the valve, 0 = Instruction is not controlling the virtual model of the valve. |
SrcQ_IO | SINT | Not Visible | Not Required | Output | Source and quality of primary input or output: 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ | SINT | Not Visible | Not Required | Output | Source and quality of primary value or status: 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
Sts_eFdbk | SINT | Not Visible | Not Required | Output | Device feedback: 0 = None/Moving/Unknown, 1 = Closed, 3 = Opened, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 8 = Clean lower seat, 10 = Clean upper seat. |
Sts_eCmd | SINT | Not Visible | Not Required | Output | Device command: 0 = None, 1 = Close, 3 = Open, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 8 = Clean lower seat, 10 = Clean upper seat. |
Sts_eSts | SINT | Not Visible | Not Required | Output | Device status: 0 = Unknown, 1 = Closed, 3 = Opened, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 8 = Clean lower seat, 10 = Clean upper seat, 11 = Moving, 12 = Pulse lower seat, 13 = Pulse upper seat, 14 = Horn, 15 = Out of service. |
Sts_eState | SINT | Not Visible | Not Required | Output | Device state for HMI state diagram: 0 = De-energized, 1 = Closed, 2 = Closed cavity outlet, 3 = Opened, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 7 = Lift lower seat for cleaning, 8 = Clean lower seat, 9 = Lift upper seat for cleaning, 10 = Clean upper seat. |
Sts_eFault | SINT | Not Visible | Not Required | Output | Device fault status: 0 = None, 16 = Position fail, 32 = I/O fault, 34 = Configuration error. |
Sts_eOutState | SINT | Not Visible | Not Required | Output | State of outputs to physical device: 0 = De-energized, 1 = Close, 2 = Close cavity outlet, 3 = Open, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 7 = Lift lower seat for cleaning, 8 = Clean lower seat, 9 = Lift upper seat for cleaning, 10 = Clean upper seat, 11 = Horn. |
Sts_eNotify | SINT | Not Visible | Not Required | Output | Summary alarm status: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyAll | SINT | Not Visible | Not Required | Output | Summary alarm status including related objects: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyIOFault | SINT | Not Visible | Not Required | Output | I/O fault alarm status: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyFail | SINT | Not Visible | Not Required | Output | Position fail alarm status: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyIntlkTrip | SINT | Not Visible | Not Required | Output | Interlock trip alarm status: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_UnackAlmCount | SINT | Not Visible | Not Required | Output | Count of unacknowledged alarms. |
Sts_eSrc | INT | Not Visible | Not Required | Output | Current command source: 0 = Logic not in use, 4 = Hand, 8 = Maintenance, 16 = Override, 32 = Program, 33 = Program Locked, 34 = Program default (Normal), 64 = Operator, 65 = Operator Locked, 66 = Operator default (Normal), 128 = Maintenance Out of Service, 129 = Programmed Out of Service (EnableIn false), 256 = External. |
Sts_bSrc | INT | Not Visible | Not Required | Output | Active command source selections (bitmapped, for HMI): .0 = Hand, .1 = Programmed Out of Service (EnableIn false), .2= Maintenance Out of Service, .3 = Maintenance, .4 = Override, .5 = External, .6 = Program Locked, .7 = Program (unlocked), .8 = Operator Locked, .9 = Operator (unlocked). |
Sts_Available | BOOL | Not Visible | Not Required | Output | 1 = Valve has been acquired by Program and is ready and available for control. |
Sts_OpenIntlkAvailable | BOOL | Not Visible | Not Required | Output | 1 = Valve can be acquired by Program and is available to open when open interlocks are OK. |
Sts_LowerSeatIntlkAvailable | BOOL | Not Visible | Not Required | Output | 1 = Valve can be acquired by Program and is available to lift lower seat when lower seat interlocks are OK. |
Sts_UpperSeatIntlkAvailable | BOOL | Not Visible | Not Required | Output | 1 = Valve can be acquired by Program and is available to lift upper seat when upper seat interlocks are OK. |
Sts_CavityIntlkAvailable | BOOL | Not Visible | Not Required | Output | 1 = Valve can be acquired by Program and is available to clean seat or cavity when cavity interlocks are OK. |
Sts_Bypass | BOOL | Not Visible | Not Required | Output | 1 = Bypassable interlocks and permissives are bypassed. |
Sts_BypActive | BOOL | Visible | Not Required | Output | 1 = Interlock/permissive bypassing is active (bypassed by command or in Maintenance command source). |
Sts_MaintByp | BOOL | Not Visible | Not Required | Output | 1 = Device has a maintenance bypass function active. |
Sts_NotRdy | BOOL | Visible | Not Required | Output | 1 = Device not ready, see Sts_NrdyXxx detail bits for reason. |
Sts_NrdyCfgErr | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, configuration error. |
Sts_NrdyFail | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, position fail, shed requires reset. |
Sts_NrdyOpenIntlk | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, open interlock not OK, valve cannot open, and if opened, valve will close. |
Sts_NrdyLowerSeatIntlk | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, lower seat interlock not OK, valve cannot lift or clean lower seat, and if seat lifted, valve will close. |
Sts_NrdyUpperSeatIntlk | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, upper seat interlock not OK, valve cannot lift or clean upper seat, and if seat lifted, valve will close. |
Sts_NrdyCavityIntlk | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, cavity Interlock not OK, valve cannot clean cavity or seats, and if cleaning, valve will close. |
Sts_NrdyIOFault | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, I/O fault, shed requires reset. |
Sts_NrdyOoS | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, device is Out of Service. |
Sts_NrdyPrioClose | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, Operator or External priority Close Command, shed requires reset. |
Sts_NrdyVirtualPhysical | BOOL | Not Visible | Not Required | Output | 1 = Device not ready, valve is transitioning between physical and virtual operation. |
Sts_Err | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration, see Sts_ErrXxx detail bits for reason. |
Sts_ErrAlm | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration, Logix tag-based alarm settings invalid. |
Sts_bErrFdbkTime | INT | Not Visible | Not Required | Output | Error in configuration, bit = 1 indicates which state’s Cfg_FdbkTimeStX is invalid. Valid = 0.0 to 60.0. |
Sts_ErrOpenPulseTime | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration, Cfg_OpenPulseTime invalid. Valid = 0.0 to 2147483.0. |
Sts_ErrClosePulseTime | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration, Cfg_ClosePulseTime invalid. Valid = 0.0 to 2147483.0. |
Sts_ErrFailTime | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration, Cfg_FailTime invalid. Valid = 0.0 to 2147483.0. |
Sts_Hand | BOOL | Visible | Not Required | Output | 1 = Hand command source is selected. |
Sts_OoS | BOOL | Visible | Not Required | Output | 1 = Out of Service command source is selected. |
Sts_Maint | BOOL | Visible | Not Required | Output | 1 = Maintenance command source is selected. |
Sts_Ovrd | BOOL | Visible | Not Required | Output | 1 = Override command source is selected. |
Sts_Ext | BOOL | Visible | Not Required | Output | 1 = External command source is selected. |
Sts_Prog | BOOL | Visible | Not Required | Output | 1 = Program (unlocked) command source is selected. |
Sts_ProgLocked | BOOL | Not Visible | Not Required | Output | 1 = Program Locked command source is selected. |
Sts_Oper | BOOL | Visible | Not Required | Output | 1 = Operator (unlocked) command source is selected. |
Sts_OperLocked | BOOL | Not Visible | Not Required | Output | 1 = Operator Locked command source is selected. |
Sts_ProgOperSel | BOOL | Not Visible | Not Required | Output | Program/Operator selection (latch) state: 1 = Program, 0 = Operator. |
Sts_ProgOperLock | BOOL | Visible | Not Required | Output | Program/Operator lock (latch) state: 1 = Locked, 0 = Unlocked. |
Sts_Normal | BOOL | Not Visible | Not Required | Output | 1 = Selected command source is the normal source (Program or Operator). |
Sts_ExtReqInh | BOOL | Not Visible | Not Required | Output | 1 = External command source selection is inhibited, External is not available in current state. |
Sts_ProgReqInh | BOOL | Not Visible | Not Required | Output | 1 = Program command source selection is inhibited, Program is not available in current state. |
Sts_MAcqRcvd | BOOL | Not Visible | Not Required | Output | 1 = Command to acquire Maintenance command source was received this scan. |
Sts_CmdConflict | BOOL | Not Visible | Not Required | Output | 1 = Conflicting commands received this scan. |
Sts_Alm | BOOL | Not Visible | Not Required | Output | 1 = An alarm is active. |
Sts_AlmInh | BOOL | Not Visible | Not Required | Output | 1 = An alarm is shelved or disabled. |
Sts_IOFault | BOOL | Not Visible | Not Required | Output | 1 = I/O communication fault. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVLVMP_Tag.@Alarms.Alm_IOFault.AlarmElement. |
Sts_Fail | BOOL | Visible | Not Required | Output | 1 = Valve position failure. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVLVMP_Tag.@Alarms.Alm_Fail.AlarmElement. |
Sts_IntlkTrip | BOOL | Not Visible | Not Required | Output | 1 = Valve closed by an interlock not OK. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVLVMP_Tag.@Alarms.Alm_IntlkTrip.AlarmElement. |
Sts_RdyAck | BOOL | Not Visible | Not Required | Output | 1 = An alarm is ready to be acknowledged. |
Sts_RdyReset | BOOL | Visible | Not Required | Output | 1 = A latched alarm or shed condition is ready to be reset. |
XRdy_Acq | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Acq, enable HMI button. |
XRdy_Rel | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Rel, enable HMI button. |
XRdy_Close | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Close, enable button. |
XRdy_Open | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Open, enable button. |
XRdy_LiftLower | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_LiftLower, enable button. |
XRdy_LiftUpper | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_LiftUpper, enable button. |
XRdy_CleanCavity | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_CleanCavity, enable button. |
XRdy_CleanLower | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_CleanLower, enable button. |
XRdy_CleanUpper | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_CleanUpper, enable button. |
XRdy_Reset | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Reset, enable button. |
XRdy_ResetAckAll | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_ResetAckAll, enable button. |
Val_Owner | DINT | Not Visible | Not Required | Output | Current object Owner ID, 0 = not owned. |
Private Input Members | Data Type | Description |
---|---|---|
CmdSrc | P_COMMAND_SOURCE | Command source selection. |
MCmd_Acq | BOOL | Maintenance Command to acquire Maintenance command source. The instruction clears this operand automatically. Default is false. |
MCmd_Bypass | BOOL | Maintenance Command to bypass all bypassable interlocks and permissives. The instruction clears this operand automatically. Default is false. |
MCmd_Check | BOOL | Maintenance Command to remove bypass and check all interlocks and permissives. The instruction clears this operand automatically. Default is false. |
MCmd_IS | BOOL | Maintenance Command to select In Service. The instruction clears this operand automatically. Default is false. |
MCmd_OoS | BOOL | Maintenance Command to select Out of Service. The instruction clears this operand automatically. Default is false. |
MCmd_Physical | BOOL | Maintenance Command to select Physical device operation. The instruction clears this operand automatically. Default is false. |
MCmd_Rel | BOOL | Maintenance Command to release Maintenance command source. The instruction clears this operand automatically. Default is false. |
MCmd_ToggleLocator | BOOL | Maintenance Command to toggle on/off valve locator/beacon. Default is false. |
MCmd_Virtual | BOOL | Maintenance Command to select Virtual device operation. The instruction clears this operand automatically. Default is false. |
OCmd_CleanCavity | BOOL | Operator Command to clean valve leakage cavity. The instruction clears this operand automatically. Default is false. |
OCmd_CleanLower | BOOL | Operator Command to clean valve lower seat. The instruction clears this operand automatically. Default is false. |
OCmd_CleanUpper | BOOL | Operator Command to clean valve upper seat. The instruction clears this operand automatically. Default is false. |
OCmd_Close | BOOL | Operator Command to close valve. The instruction clears this operand automatically. Default is false. |
OCmd_LiftLower | BOOL | Operator Command to lift lower valve seat. The instruction clears this operand automatically. Default is false. |
OCmd_LiftUpper | BOOL | Operator Command to lift upper valve seat. The instruction clears this operand automatically. Default is false. |
OCmd_Lock | BOOL | Operator Command to select Operator Locked command source and disallow Program. The instruction clears this operand automatically. Default is false. |
OCmd_Normal | BOOL | Operator Command to select configured normal command source (Operator or Program). The instruction clears this operand automatically. Default is false. |
OCmd_Open | BOOL | Operator Command to open valve. The instruction clears this operand automatically. Default is false. |
OCmd_Oper | BOOL | Operator Command to select Operator (unlocked) command source. The instruction clears this operand automatically. Default is false. |
OCmd_Prog | BOOL | Operator Command to select Program (unlocked) command source. The instruction clears this operand automatically. Default is false. |
OCmd_Reset | BOOL | Operator Command to reset shed latches and returned-to-normal latched alarms. The instruction clears this operand automatically. Default is false. |
OCmd_ResetAckAll | BOOL | Operator Command to acknowledge all alarms and reset latched alarms and shed conditions. The instruction clears this operand automatically. Default is false. |
OCmd_Unlock | BOOL | Operator Command to unlock Operator command source and allow Program to acquire. The instruction clears this operand automatically. Default is false. |
Private Output Members | Data Type | Description |
---|---|---|
HMI_BusObjIndex | DINT | This object's index in the bus array, for use by HMI display. |
HMI_eCmdState | SINT | Command to valve, for use on HMI/dialog: 0 = None, 1 = Close, 3 = Open, 4 = Lift lower seat, 5 = Lift upper seat, 6 = Clean cavity, 8 = Clean lower seat, 10 = Clean upper seat. |
MRdy_Acq | BOOL | 1 = Ready for MCmd_Acq, enable HMI button. |
MRdy_Bypass | BOOL | 1 = Ready for MCmd_Bypass, enable HMI button. |
MRdy_Check | BOOL | 1 = Ready for MCmd_Check, enable HMI button. |
MRdy_IS | BOOL | 1 = Ready for MCmd_IS, enable HMI button. |
MRdy_OoS | BOOL | 1 = Ready for MCmd_OoS, enable HMI button. |
MRdy_Physical | BOOL | 1 = Ready for MCmd_Physical, enable HMI button. |
MRdy_Rel | BOOL | 1 = Ready for MCmd_Rel, enable HMI button. |
MRdy_ToggleLocator | BOOL | 1 = Ready for MCmd_ToggleLocator, enable HMI button. |
MRdy_Virtual | BOOL | 1 = Ready for MCmd_Virtual, enable HMI button. |
ORdy_CleanCavity | BOOL | 1 = Ready for OCmd_CleanCavity, enable HMI button. |
ORdy_CleanLower | BOOL | 1 = Ready for OCmd_CleanLower, enable HMI button. |
ORdy_CleanUpper | BOOL | 1 = Ready for OCmd_CleanUpper, enables HMI button. |
ORdy_Close | BOOL | 1 = Ready for OCmd_Close, enable HMI button. |
ORdy_LiftLower | BOOL | 1 = Ready for OCmd_LiftLower, enable HMI button. |
ORdy_LiftUpper | BOOL | 1 = Ready for OCmd_LiftUpper, enable HMI button. |
ORdy_Lock | BOOL | 1 = Ready for OCmd_Lock, enable HMI button. |
ORdy_Normal | BOOL | 1 = Ready for OCmd_Normal, enable HMI button. |
ORdy_Open | BOOL | 1 = Ready for OCmd_Open, enable HMI button. |
ORdy_Oper | BOOL | 1 = Ready for OCmd_Oper, enable HMI button. |
ORdy_Prog | BOOL | 1 = Ready for OCmd_Prog, enable HMI button. |
ORdy_Reset | BOOL | 1 = Ready for OCmd_Reset, enable HMI button. |
ORdy_ResetAckAll | BOOL | 1 = Ready for OCmd_ResetAckAll, enable HMI button. |
ORdy_Unlock | BOOL | 1 = Ready for OCmd_Unlock, enable HMI button. |
Public InOut Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
BusObj | BUS_OBJ | Visible | Required | InOut | Bus component |
BUS_OBJ Structure
The BUS_OBJ structure links the device to other devices and instructions in a complex control strategy, typically into a hierarchy. A Bus Object rolls up status and alarm information from lower level devices to higher level control and fans out commands from higher level control to lower level devices, and items link to the bus by referencing a single member of the BUS_OBJ array associated with the bus.
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, the Bus functions of this instruction are not available.
Members | Data Type | Description |
---|---|---|
Inp_Cmd | DINT | Input to assert commands |
Out_Cmd | DINT | Resultant commands |
Inp_CmdLLH | DINT | Input for level normally high commands |
Out_CmdLLH | DINT | Resultant line level high commands |
Inp_Sts | DINT | Input to assert status |
Out_Sts | DINT | Resultant status |
Inp_CmdAck | DINT | Input to assert a command acknowledgement |
Out_CmdAck | DINT | Resultant command acknowledgements |
Inp_SeverityMax | DINT | Input: maximum alarm severity |
Out_SeverityMax | DINT | Resultant of maximum alarm severity |
Cfg_CmdMask | DINT | Propagation mask for commands |
Cfg_CmdLLHMask | DINT | Propagation mask for line level high commands |
Cfg_StsMask | DINT | Propagation mask for status |
Ref_Index | DINT | Bus array index |
Alarms
Discrete
Logix Designer
tag-based alarms are defined for these members:Member | Alarm Name | Description |
---|---|---|
Sts_IntlkTrip | Alm_IntlkTrip | Device de-energized or set to Position 1 by an interlock Not OK. |
Sts_IOFault | Alm_IOFault | I/O fault. |
Sts_Fail | Alm_Fail | Device failure. |
Mark the alarm as used or unused and set standard configuration members of the discrete Logix Tag based alarm. Use this format to access alarm elements:
Tag.@Alarms.AlarmName.AlarmElement
The PVLVMP instruction uses these alarms:
- Raises the Interlock Trip alarm when an interlock not-OK condition occurs for a particular state and the device is currently commanded to that state. The device will be commanded to close when an interlock trip occurs. If interlocks are not bypassed, a bypassable interlock or a non-bypassable interlock not-OK condition initiates an interlock trip. If interlocks are bypassed, only a non-bypassable interlock not-OK condition initiates an interlock trip.
- Raises the I/O Fault alarm when the Inp_IOFault input is true. This input is usually used to indicate to the instruction that a communication failure has occurred for its I/O. If the I/O Fault is configured as a shed fault, the device will be commanded to close and will remain closed until reset.
- Raises the Fail alarm when the valve is commanded to a new position and the device feedbacks fail to confirm that the valve reached each required position within the configured failure time. If the Failure is configured as a shed fault, the valve will be commanded closed and cannot be opened until reset.
Program, Operator, and External commands reset latched alarms, and reset and acknowledge all alarms of the instruction (Alarm Set) at the same time. This diagram shows how the commands interact with the PVLVMP instruction.

Operation
The PVLVMP instruction operates by using a state model, as shown in this diagram.

This diagram illustrates functionality of the PVLVMP instruction.

This diagram shows logic of interlocks associated with commands of the PVLVMP instruction.

Operator command request confirmation
The PVLVMP instruction enables these operator commands and settings:
- OCmd_CleanCavity
- OCmd_CleanLower
- OCmd_CleanUpper
- OCmd_Close
- OCmd_LiftLower
- OCmd_LiftUpper
- OCmd_Open
Enforced security might require the request to be confirmed or canceled before the selected command executes or setting is accepted. The instruction checks the security rules by inspecting Cfg_CnfrmReqd. If Cfg_CnfrmReqd = 0, no confirmation is required and the request executes immediately. If Cfg_CnfrmReqd = 1, the instruction waits for operator confirmation or cancelation of the command. If Cfg_CnfrmReqd = 2 or 3, eSignature is needed before command confirmation is enabled.
Virtualization
Use virtualization for instruction testing and operator training. Command virtual operation using program command PCmd_Virtual or maintenance command MCmd_Virtual. After finishing virtual operation, use program command PCmd_Physical or maintenance command MCmd_Physical to return to normal physical device operation.
When Virtualization is active, the device outputs of the PVLVMP instruction hold at 0, virtual feedback of a working device is provided, and I/O faults are ignored. Manipulate the instruction to operate as if a working valve is present.
Initialization
The instruction is normally initialized in the instruction first run. Request re-initialization by setting Inp_InitializeReq = 1. For proper initialization, when adding the instruction while performing an online edit of the code, make sure that Inp_InitializeReq = 1, the default value.
Configuration of Strings for HMI
Configure strings for HMI faceplates, displayed in
FactoryTalk View
, and for the Logix Designer
configuration dialog box. The strings are set to extended properties of tag items.- Description
- Label for graphic symbol
- Display Library for HMI Faceplate call-up
- Instruction name
- Area name
- URL link
- Navigation to an object with more information
- Name of Interlock Trip Alarm
- Name of I/O Fault Alarm
- Name of Fail Alarm
Command Source
The instruction uses these command sources. The command sources are prioritized in order from highest to lowest in this table.
Command Source | Description |
---|---|
Hand | Hardwired logic or other logic outside the instruction controls the device. The instruction tracks the state of the device for bumpless transfer back to one of the other command sources. This is the highest priority command source. |
Out-of-Service | The instruction is disabled. Outputs are de-energized. Valve commands from any source are discarded. On return to In Service, the valve is commanded closed. |
Maintenance | Maintenance controls the device and supersedes Operator, Program, External and Override control. Operator commands and settings from the HMI are accepted. |
Override | Priority logic controls the device and supersedes Operator, Program and External control. Override Input (Inp_Ovrd) is accepted. |
External | External logic (for example, field pilot control or upstream SCADA) controls the device. External commands (XCmd_) are accepted. |
Program locked | Program logic controls the device. Program commands (PCmd_) are accepted. Operator cannot take control from the Program. Override cannot take control from theProgram unless Cfg_OvrdOverLock = 1. |
Program | Program logic controls the device. Program commands (PCmd_) are accepted. |
Operator locked | The Operator controls the device. Operator commands (OCmd_) from the HMI are accepted. Program cannot take control from Operator. Override cannot take control from Operator unless Cfg_OvrdOverLock = 1. |
Operator | The Operator controls the device. Operator commands (OCmd_) from the HMI are accepted. This is the lowest priority command source. |
The instruction enables or disables these operations:
- Maintenance Out-of-Service exists
- Maintenance exists
- External exists
- Program (unlocked) exists
- Program locked exists
- Operator (unlocked) exists
- Operator locked exists
- PCmd_Lock used as a Level (1 = Lock, 0 = Unlock)
The instruction checks for invalid configurations of control and forces the nearest valid configuration.
The core control model arbitrates the source of the commands and parameters that the receiving function accepts. The core control model determines if the source is:
- A programmatic entity which resides entirely within the processing environment, or
- An external interface entity which issues commands and parameters external and asynchronously to the processing environment.
Locking a control source prevents the other control source from acquiring privilege.
Core Command Source Model
The core control model consists of these control sources:
- Oper
- OperLocked
- Prog
- ProgLocked
The control model defaults to this configuration. Other control sources may be present in the model but act as overriding control sources, acting independent of the base Operator/Program state machine.
Enable control sources as Configuration
The user can enable and disable individual control sources. The default configuration uses the entire base model; upon power-up of the processing environment the control source will be the designated default. Some combinations of enabled control sources are disallowed as they are either unnecessary or could create unintended changes.
Prog Power Up
Configuration allows the user to specify whether Operator or Program is the power-up default.
Prog Priority
Configuration allows the user to specify whether Operator or Program commands take priority when simultaneously asserted.
Automatic reset of commands
All commands are treated as one-shot-latched. Commands are automatically cleared when the instruction executes and processes them.
Change Destination States
Under certain configurations the destination command source for some commands may change. This is in keeping with the intent of the command. For example, if the Program state is disabled, the destination of the OCmd_Prog command becomes the Program Locked state instead of the Program state. This maintains the intent of the OCmd_Prog command: the operator entity wishes to place the function in control of the program. If the command was eliminated there would be no way to accomplish this. This is only done in configurations where it would cause no conflict or race condition, but serves to preserve as much user functionality as is practical.
Higher Priority Command Sources
These Higher priority command sources operate independently within the model:
- External
- Override
- Maintenance
- Out-of-Service
- In-Service
- Hand
Monitor the PVLVMP Instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index through arrays in the Logix 5000 General Instructions manual for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | Any commands received before first scan are discarded. The device is de-energized. |
Instruction first run | Any commands received before first scan are discarded. The device is commanded to the closed state. |
Rung-condition-in is false | Handled the same as if the device is taken Out of Service by command. The device outputs are de-energized, and the device Command Source is shown as Program Out of Service on the HMI. All alarms are cleared. The rung-condition-out continues as false. |
Rung-condition-in is true | Set rung-condition-out to rung-condition-in. The instruction executes. |
Postscan | Rung-condition-out is cleared to false. |
Function Block Diagram
Condition/State | Action Taken |
---|---|
Prescan | Any commands received before first scan are discarded. The device is de-energized. |
Instruction first run | Any commands received before first scan are discarded. The device is commanded to the closed state. |
Instruction first scan | See instruction first run in the function block diagram table. |
EnableIn is false | Handled the same as if the device is taken Out of Service by command. The device outputs are de-energized, and the device Command Source is shown as Program Out of Service on the HMI. All alarms are cleared. EnableOut is set to false. |
EnableIn is true | EnableOut is set to true. The instruction executes. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic, it executes.
Condition/State | Action taken |
---|---|
Prescan | See Prescan in the Function Block Diagram table. |
Instruction first run | See Instruction first run in the Function Block Diagram table. |
EnableIn is true | See EnableIn is true in the Function Block Diagram table. |
Postscan | See Postscan in the Function Block Diagram table. |
Example
In this example, the PVLVMP instruction is used to implement a mix-proof valve feeding bulk material from a storage silo into a mixer. For this example, the mix-proof valve connects to the control system by using two inputs and three outputs. The valve state configurations are shown in these tables
State 0 (De-energized). Note: Close output is set for display purposes only:
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 1 | 0 | 0 |
Open | 0 | 0 | 0 |
Lift lower seat | 0 | 1 | 0 |
Lift upper seat | 0 | 1 | 0 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
State 1 (Close):
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 0 | 0 | 0 |
Open | 0 | 0 | 0 |
Lift lower seat | 0 | 1 | 0 |
Lift upper seat | 0 | 1 | 0 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
State 2 (Close cavity out):
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 0 | 0 | 0 |
Open | 1 | 0 | 0 |
Lift lower seat | 0 | 1 | 1 |
Lift upper seat | 0 | 1 | 1 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
State 3 (Open):
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 0 | 0 | 0 |
Open | 1 | 0 | 0 |
Lift lower seat | 0 | 1 | 1 |
Lift upper seat | 0 | 1 | 1 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
State 4 (Lift lower seat):
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 0 | 0 | 0 |
Open | 0 | 0 | 0 |
Lift lower seat | 1 | 1 | 1 |
Lift upper seat | 0 | 1 | 0 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
State 5 (Lift upper seat):
Output | Feedback | ||
---|---|---|---|
State | Required | State | |
Close | 0 | 0 | 0 |
Open | 0 | 0 | 0 |
Lift lower seat | 0 | 1 | 0 |
Lift upper seat | 1 | 1 | 1 |
Cavity in | 0 | 0 | 0 |
Cavity out | 0 | 0 | 0 |
Ladder Diagram


Function Block Diagram

Structured Text
XV5047.Inp_LowerSeatLSData:=XV5047_ZSL
XV5047.Inp_UpperSeatLSData:=XV5047_ZSU
PVLVMP(XV5047, 0);
XV5047_OP:=XV5047.Out_OpenData;
XV5047_LL:=XV5047.Out_LiftLowerData;
XV5047_LU:=XV5047.Out_LiftUpperData;
Provide Feedback