OUTPUT_CAM Structure

The OUTPUT_CAM data type is an array that defines the specifics for each Output Cam element. The OUTPUT_CAM contains the following members:
Mnemonic
Data Type
Description
OutputBit
DINT
You must select an output bit within the range of 0 to 31. A selection of less than 0 or greater than 31 results in an Illegal Output Cam error and the cam element is not considered.
LatchType
DINT
The Latch Type determines how the corresponding output bit is set. A value of less than 0 or greater than 3 results in an Illegal Output Cam error and a latch type of Inactive is used.
0 = Inactive - The output bit is not changed.
1 = Position - The output bit is set when the axis enters the compensated cam range.
2 = Enable - The output bit is set when the enable bit becomes active.
3 = Position and Enable - The output bit is set when the axis enters the compensated cam range and the enable bit becomes active.
UnlatchType
DINT
The Unlatch Type determines how the output bit is reset. Selecting a value less than 0 or greater than 5 results in an Illegal Output Cam error and an unlatch type of Inactive is used.
0 = Inactive- -The output bit is not changed.
1 = Position - The output bit is reset when the axis leaves the compensated cam range.
2 = Duration - The output bit is reset when the duration expires.
3 = Enable - The output bit is reset when the enable bit becomes inactive.
4 = Position and Enable - The output bit is reset when the axis leaves the compensated cam range or the enable bit becomes inactive.
5 = Duration and Enable - The output bit is reset when the duration expires or the enable bit becomes inactive.
Left
REAL
The left cam position along with the right cam position define the cam range of the Output Cam element. The left and right cam positions specify the latch or unlatch positions of the output bit when the latch or unlatch type is set to
Position
or
Position and Enable
with the enable bit active. If the left position is less than the Cam Start position or greater than the Cam End position, an Illegal Output Cam error is returned and the cam element is not considered.
Right
REAL
The right cam position along with the left cam position define the cam range of the Output Cam element. The right and left cam positions specify the latch or unlatch positions of the output bit when the latch or unlatch type is set to
Position
or
Position and Enable
with the enable bit active. If the right position is less than the Cam Start position or greater than the Cam End position, an Illegal Output Cam error is returned and the cam element is not considered.
Duration
REAL
Duration specifies the time in seconds between latching and unlatching when the Unlatch Type is
Duration
or
Duration and Enable
with the enable bit active. A value less than or equal to 0 results in an Illegal Output Cam error and the cam element is not considered.
EnableType
DINT
This defines the source and polarity of the specified EnableBit when LatchType or UnlatchType is
Enable
,
Position and Enable
or
Duration and Enable
. A value of less than 0 or greater than 31 results in an Illegal Output Cam error and the cam element is not considered.
0 = Input - The enable bit is in the Input parameter.
1 = Inverted Input - The enable bit is in the input parameter and is active low.
2 = Output - The enable bit is in the Output parameter.
3 = Inverted Output - The enable bit is in the Output parameter and is active low.
EnableBit
DINT
The value of the Enable Bit selected must be between 0 and 31 when LatchType or UnlatchType is
Enable
,
Position and Enable
or
Duration and Enable
. A value of less than 0 or greater than 31 results in an Illegal Output Cam error and the cam element is not considered.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal