Reset Dominant (RESD)

This information applies to the
Compact GuardLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
Compact GuardLogix
5480, and
ControlLogix
5580 controllers.
The RESD instruction uses Set and Reset inputs to control latched outputs. The Reset input has precedence over the Set input.
Available Languages
Ladder Diagram
This instruction is not available for ladder diagram.
Function Block
RESD_FBD_avail_v31
Structured Text
RESD(RESD_tag);
Operands
Function Block
Operand
Type
Format
Description
RESD tag
DOMINANT_RESET
structure
RESD structure
DOMINANT_RESET Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
Set
BOOL
Set input to the instruction.
Default is cleared.
Reset
BOOL
Reset input to the instruction.
Default is cleared.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled.
Out
BOOL
The output of the instruction.
OutNot
BOOL
The inverted output of the instruction.
Structured text
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.
Description
The Reset Dominant instruction uses the Set and Reset input parameters to control latched output parameters Out and OutNot. The Reset input has precedence over the Set input.
Out will be latched true whenever the Set input parameter is set true. Setting the Reset parameter to true will override the current state of Out, setting Out to false.
When Reset returns to false, Out will be latched to the current state of the Set input parameter. OutNot will be set to the opposite state of Out.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See
Common Attributes
for fault related attributes.
Execution
Function Block
Condition/State
Action Taken
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is false
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is true
EnableIn and EnableOut bits are set to true.
The instruction executes.
Instruction first run
Out bit is set to false. OutNot is set to true.
Instruction first scan
N/A
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal Execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Example
When Set is true and Reset is false, Out is set true. When Reset is true, Out is cleared. The Reset input has precedence over the Set input. The RESD instruction sets OutNot to the opposite state of Out.
Function Block
RESD_FBD_ex_v31
Structured Text
RESD_01.Set := set_input;
RESD_01.Reset := reset_input;
RESD(RESD_01);
out_output := RESD_01.Out;
outNot_output := RESD_01.OutNot;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal