Motion Axis Move (MAM)

CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580,
Compact GuardLogix
5380, and
GuardLogix
5580 controllers
Use the Motion Axis Move (MAM) instruction to move an axis to a specified position.
This is a transitional instruction. Follow these steps when using it:
  • In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
  • In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Architecture and safety support
Architecture
Standard
Safety
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers
Yes
No
Available Languages
Ladder Diagram
MAM_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
MAM(Axis, MotionControl, MoveType, Position, Speed, SpeedUnits, AccelRate, AccelUnits, DecelRate, DecelUnits, Profile, AccelJerk, DecelJerk, JerkUnits, Merge, MergeSpeed, LockPosition, LockDirection, EventDistance, CalculatedData);
Operands
Ladder Diagram
Operand
Type
Tip:
AXIS_CONSUMED is supported by
Compact GuardLogix
5580,
CompactLogix
5380, and
CompactLogix
5480 controllers only.
Type
Tip:
AXIS_GENERIC is supported by the
ControlLogix
5570 and the
GuardLogix
5570 controllers only.
Format
Description
Axis
AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE
Tag
Name of the axis.
For an Absolute or Incremental Master Offset move, enter the slave axis.
For controllers that support the REF_TO motion data types, the supported axis operand type can be replaced by an equivalent REF_TO type.
Motion Control
MOTION_
INSTRUCTION
MOTION_
INSTRUCTION
Tag
Control tag for the instruction
Move type
DINT
DINT
Immediate or Tag
To
Use This Move Type
And Enter
Move an axis to an absolute position
Absolute
0
Move an axis a specified distance from where it is now
Incremental
1
Move a Rotary axis to an absolute position in the shortest
direction regardless of its current position
Rotary Shortest Path
2
Move a Rotary axis to an absolute position in the
positive
direction regardless of its current position
Rotary Positive
3
Move a Rotary axis to an absolute position in the
negative
direction regardless of its current position
Rotary Negative
4
Offset the master value of a position cam to an absolute position
Absolute Master Offset
5
Offset the master value of a position cam by an incremental distance
Incremental Master Offset
6
See Choose a Move Type for a Rotary Axis below for more information about rotary moves.
Position
REAL
REAL
Immediate or Tag
Absolute position or incremental distance for the move
For This Move Type
Enter This Position Value
Absolute
Position to Move to
Incremental
Distance to Move
Rotary Shortest Path
Position to move to. Enter a positive value that is less than the Position Unwind value.
Rotary Positive
Rotary Negative
Absolute Master Offset
Absolute Offset Position
Incremental Master Offset
Incremental Offset Distance
Speed
REAL
REAL
Immediate or Tag
Speed to move the axis in Speed Units
Speed Units
DINT
DINT
Immediate
Which units do you want to use for the Speed?
Units per sec (0)
% of Maximum (1)
Time (3)
Units per MasterUnit (4)
Master Units (7)
Accel Rate
REAL
REAL
Immediate or Tag
Acceleration rate of the axis in Accel Units
Accel Units
DINT
DINT
Immediate
Which units do you want to use for the Accel Rate?
Units per sec
2
(0)
% of Maximum (1)
Time (3)
Units per MasterUnit
2
(4)
Master Units (7)
Decel Rate
REAL
REAL
Immediate or Tag
Deceleration rate of the axis in Deceleration Units.
Decel Units
DINT
DINT
Immediate
Which units do you want to use for the Decel Rate?
Units per sec
2
(0)
% of Maximum (1)
Time (3)
Units per MasterUnit
2
(4)
Master Units (7)
Profile
DINT
DINT
Immediate
Select the velocity profile to run for the move:
  • Trapezoidal (0)
  • S-Curve (1)
Accel Jerk
REAL
REAL
Immediate or Tag
The instruction only uses the jerk operands if the Profile is S-curve. You must always fill them in however.
  • Accel Jerk is the acceleration jerk rate for the axis.
  • Decel Jerk is the deceleration jerk rate for the axis.
Use these values to get started.
  • Accel Jerk = 100
  • Decel Jerk = 100
  • Jerk Units = 2 (% of Time)
You can also enter the jerk rates in these Jerk Units.
  • Units per sec
    3
    (0)
  • % of Maximum (1)
  • % of Time (2)
  • Time (3)
  • Units per MasterUnit
    3
    (4)
  • % of Time-Master Driven (6)
  • Master Units (7)
Decel Jerk
REAL
REAL
Immediate or Tag
Jerk Units
DINT
DINT
Immediate
Merge
DINT
DINT
Immediate
Do you want to turn all current axis motion into a pure move governed by this instruction regardless of the motion instructions currently in process?
  • NO— Choose Disabled (0)
  • YES — Choose Enabled (1)
Merge Speed
DINT
DINT
Immediate
If Merge is Enabled, which speed do you want to move at?
  • Speed of this instruction — Select Programmed (0)
  • Current speed of the axis — Select Current (1)
Lock Position
REAL
REAL
Immediate or Tag
Position on the Master Axis where a Slave should start following the master after the move has been initiated on the Slave Axis.
See the Structure section below for more information.
Lock Direction
SINT, INT or DINT
SINT, INT or DINT
Immediate
Specifies the conditions when the Lock Position should be used.
Valid Values = 0-4
Default = None
(Enumeration 1-4 are currently not allowed in Time Driven or Time Based modes.)
See the Structure section below for more information.
Event Distance
REAL
ARRAY or 0
REAL
ARRAY or 0
Array Tag
The position(s) on a move measured from the end of the move.
See the Structure section below for more information.
Calculated Data
REAL
ARRAY or 0
REAL
ARRAY 0
Array Tag
Master Distance(s) (or time) needed from the beginning of the move to the Event Distance point.
See the Structure section below for more information.
Structured Text
This Operand
Has These Options Which You
Enter as Text
Or Enter as a Number
SpeedUnits
unitspersec
%ofmaximum
time
unitspermasterunit
masterunits
0
1
3
4
7
AccelUnits
unitspersec
2
%ofmaximum
time
unitspermasterunit
2
masterunits
0
1
3
4
7
DecelUnits
unitspersec
2
%ofmaximum
time
unitspermasterunit
2
masterunits
0
1
3
4
7
Profile
trapezoidal
scurve
0
1
JerkUnits
unitspersec
3
%ofmaximum
%oftime
time
unitspermasterunit
3
%oftime-masterdriven
masterunits
0
1
2
3
4
6
7
Merge
disabled
enabled
0
1
MergeSpeed
programmed
current
0
1
Lock Position
No enumeration
Immediate, Real, or Tag
Lock Direction
None
immediateforwardonly
immediatereverseonly
positionforward
positionreverse
0
1
2
3
4
Event Distance
No enumeration
Array or 0
Calculated Data
No enumeration
Array or 0
See Structured Text Syntax for more information on the syntax of expressions within structured text.
MOTION_INSTRUCTION Data Type
To See If
Check If This Bit Is Set To
Data Type
Notes
A false-to-true transition caused the instruction to execute
EN
BOOL
The EN bit stays set until the process is complete and the rung goes false.
The move was successfully initiated
DN
BOOL
An error happened
ER
BOOL
The axis is moving to the end Position
IP
BOOL
Any of these actions stop this move and clear the IP bit:
  • The axis gets to the end Position
  • Another MAM instruction supersedes this MAM instruction
  • MAS instruction
  • Merge from another instruction
  • Shutdown command
  • Fault Action
The axis is at the end Position
PC
BOOL
  • The PC bit stays set until the rung makes a false-to-true transition.
  • The PC bit stays cleared if some other action stops the move before the axis gets to the end Position.
Description
The MAM instruction moves an axis to either a specified absolute position or by a specified incremental distance. The MAM instruction can also produce other special types of moves.
Trapezoidal Move Starting from Standstill
MamTrap
Programming Guidelines
WARNING:
Risk of Velocity and/or End Position Overshoot
If you change move parameters dynamically by any method, that is by changing move dynamics [Motion Change Dynamics (MCD)] instruction or by starting a new instruction before the last one has completed, be aware of the risk of velocity and/or end position overshoot.
A Trapezoidal velocity profile can overshoot if maximum deceleration is decreased while the move is decelerating or is close to the deceleration point.
An S-curve velocity profile can overshoot if:
  1. maximum deceleration is decreased while the move is decelerating or close to the deceleration point; or
  2. maximum acceleration jerk is decreased and the axis is accelerating. Keep in mind, however, that jerk can be changed indirectly if it is specified in % of time.
For more information, see Troubleshoot Axis Motion
Guideline
Details
In ladder diagram, toggle the rung condition each time you want to execute the instruction.
This is a transitional instruction.
In ladder diagram, toggle the rung-condition-in from cleared to set each time you want to execute the instruction.
In structured text, condition the instruction so that it only executes on a transition
In structured text, instructions execute each time they are scanned.
Condition the instruction so that it only executes on a transition. Use either of these methods:
  • qualifier of an SFC action
  • structured text construct
For more information, see Structured Text Syntax.
For a Master Offset move, enter the slave axis but use master units.
Use an Absolute or Incremental Master Offset move to off set the master value of a position cam without actually changing the position of the master axis. This shifts the position cam profile along the master axis.
  • For Axis, enter the slave axis.
  • For Position, enter the absolute offset position or incremental offset distance
  • For Speed, Acceleration, Deceleration, and Jerk, enter them for the master axis.
The instruction adds in the offset at the Speed, Acceleration, Deceleration, and Jerk values.
Use % of Time for the easiest programming and tuning of jerk
For an easy way to program and tune jerk, enter it as a % of the acceleration or deceleration time.
For more information, see Tune an S-Curve Profile.
Use Merge to cancel the motion of other instructions
How you want to handle any motion that’s already in process?
If you want to
And you want to
Then set
Add the move to any motion already in process
arrow_right (2)
Merge = Disabled
Merge Speed = Programmed
The instruction ignores Merge Speed but you must fill it in anyway.
End the motion from other instructions and just jog
Move at the Speed that you set in this instruction
Merge = Enabled
Merge Speed = Programmed
Move at the speed that the axis is already moving
Merge = Enabled
Merge Speed = Current
The instruction ignores the value that you put in the Speed operand.
Is This an Absolute or Incremental Master Offset Move?
If this is an Absolute or Incremental Master Offset move and Merge is Enabled, then the following is true.
  • The move
    only
    ends an Absolute or Incremental Master Offset move that is already in process.
  • The move
    does not
    affect any other motion that is already in process.
Use a second MAM instruction to change one that is already in process.
You can change the position, speed, acceleration, or deceleration. The change immediately takes effect.
To Change the Position of An
Set Up a Second MAM Instruction Like This
Absolute Move
Either:
  • Set the Move Type to Absolute and the Position to the new position.
  • Set the Move Type to Incremental and set the Position to the distance to change the end position. The new end position is the old end position plus the new incremental distance.
In either case, the axis moves to the new position without stopping at the old position—including any required change of direction.
Incremental Move
Either:
  • Set the Move Type to Absolute and the Position to the new position. The axis goes directly to the new position without completing the incremental move.
  • Set the Move Type to Incremental and set the Position to the additional distance. The axis moves the total of both incremental moves.
Combine a move with gearing for complex profiles and synchronization.
You can use a Motion Axis Gear (MAG) instruction together with an MAM instruction. This superimposes the gearing on top of the move or the move on top of the gearing.
Example:
Superimpose an incremental move on top of electronic gearing for phase advance and retard control.
Choose a Move Type for a Rotary Axis
Move Type
Example
Description
Absolute
Absolute move to 225°. The direction depends on the starting position of the axis.
shrtpth1
With an Absolute move, the direction of travel depends on the current position of the axis and is not necessarily the shortest path to the end position. Starting positions less than the end position result in motion in the positive direction, while starting positions greater than the end position result in motion in the negative direction.
The specified position is interpreted trigonometrically and can be positive or negative. It can also be greater than the Position Unwind value. Negative position values are equivalent to their corresponding positive values and are useful when rotating the axis through 0. For example, –90° is the same as +270°. When the position is greater than or equal to the Position Unwind value, the axis moves through more than one revolution before stopping at an absolute position.
Incremental
The specified distance is interpreted trigonometrically and can be positive or negative. It can also be greater than the Position Unwind value. When the distance is greater than the Position Unwind value, the axis moves through more than one revolution before stopping.
Rotary Shortest Path
Rotary Shortest Path move from 30° to 225°.
shrtpth2
Important:
Only use a Rotary Shortest Path move if the Positioning Mode of the axis is Rotary (Rotary axis).
A Rotary Shortest Path move is a special type of absolute move for a Rotary axes. The axis moves:
  • To the specified Position in the
    shortest
    direction regardless of its current position
  • Through 0° if needed.
With a Rotary Shortest Path move, you:
  • Can start the move while the axis is moving or standing still
  • Cannot
    move the axis more than one revolution with a single move.
Rotary Positive
Rotary Positive move from 315° to 225°.
rotaryposmove
Important:
Only use a Rotary Positive move while the axis is standing still and not moving. Otherwise the axis could move in the wrong direction.
A Rotary Positive move is a special type of absolute move for a Rotary axis.
The axis:
  • Moves to the specified Position in the
    positive
    direction regardless of its current position
  • Moves through 0° if needed
You can’t move the axis more than one revolution with a single Rotary Shortest Path move.
Rotary Negative
Rotary Negative move from 45° to 225°.
rotarynegmove
Important:
Only use a Rotary Shortest Path move if
  • The Positioning Mode of the axis is Rotary (Rotary axis).
  • The axis is standing still and not moving. Otherwise the axis could move in the wrong direction.
A Rotary Negative move is a special type of absolute move for a Rotary axis. The axis:
  • Moves to the specified Position in the
    negative
    direction regardless of its current position
  • Moves through 0° if needed
You cannot move the axis more than one revolution with a single Rotary Shortest Path move.
When MAM (Merge = Enabled) is used on any axis associated with a coordinate system and a coordinated motion instruction is running on it, Coordinate system’s maximum deceleration is used to stop remaining axes. If the coordinate system contains orientation axes, Coordinate system’s Orientation maximum deceleration is used for stopping remaining Rx, Ry or Rz axes.
Structure
See Input and Output Parameters Structure for Single Axis Motion Instructions for the input and output parameters that are available for the MAM instruction via the Master Driven Speed Control (MDSC) function. Before any of these parameters is active, you must execute an MDAC instruction and it must be active (IP bit is set).
Affected Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or a reference of incorrect type is passed to the Axis Operand. See Common Attributes for operand-related faults.
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, .ER, and .IP bits are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if the .DN or .ER bit is true.
Rung-condition-out is true
The .EN bit is set to true and the instruction executes.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table
Normal execution
See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Error Codes
See Error Codes (.ERR) for Motion Instructions.
Runtime Error Condition
The slave move must start at rest if Speed Units = Seconds or Master Units. This condition may occur when the MAM with Speed = Seconds or Master Units is started while another MAM is in progress (merging or replacement mode).
Extended Error Codes
Use Extended Error Codes (EXERR) for more instruction about an error. See Error Codes (.ERR) for Motion Instructions.
If ERR is
And EXERR is
Then
Cause
Corrective Action
13
Varies
An operand is outside its range.
The EXERR is the number of the operand that is out of range. The first operand is 0.
For example, if EXERR = 4, then check the Speed.
EXERR
Operand
0
Axis
1
Motion Control
2
Move Type
3
Position
4
Speed
6
Accel Rate
8
Decel Rate
15
-1
The coordinate system has a Maximum Deceleration of 0.
Go to the Properties for the coordinate system axis and set a Maximum Deceleration.
0 or more
An axis in the coordinate system has a Maximum Deceleration of 0.
  1. Open the Properties for the axis.
  2. Use the EXERR value to see which axis has the Maximum Deceleration of 0.
  3. The axis that you are moving via the MAM instruction has a deceleration rate of 0.
Changes to Status Bits
Motion Instruction Predefined Data Type Status Bits
See Status Bits for Motion Instructions (MAM, MATC, MAJ) When MDAC Is Active.
MAM Changes to Single Axis Status Bits
Bit Name
Meaning
MotionStatus
The motion status bit for your axis.
Bit Number
Meaning
AccelStatus
0
The axis is not accelerating (FALSE state).
DecelStatus
1
The axis is not decelerating (FALSE state).
MoveStatus
2
The axis is not moving (FALSE state).
JogStatus
3
The axis is not jogging (FALSE state).
GearingStatus
4
The axis is not gearing (FALSE state).
HomingStatus
5
The axis is not homing (FALSE state).
StoppingStatus
6
The axis is stopping (TRUE state).
AxisHomedStatus
7
The axis is not homed (FALSE state).
PositionCamStatus
8
The axis is not position camming (FALSE state).
TimeCamStatus
9
The axis is not time camming (FALSE state).
PositionCamPendingStatus
10
The axis does not have a Position Cam Pending (FALSE state).
TimeCamPendingStatus
11
The axis does not have a Time Cam Pending (FALSE state).
GearingLockStatus
12
The axis is not in a Gear Locked condition (FALSE state).
PositionCamLockStatus
13
The axis is not in a Position Cam Locked condition (FALSE state).
TimeCamLockStatus
14
The axis is not in a Time Cam Locked condition (FALSE state).
MasterOffsetMoveStatus
15
The axis is offset (TRUE state).
CoordinatedMotionStatus
16
Sets when the MDAC instruction executes (TRUE state). Clears when the instruction completes (FALSE state).
TransformStateStatus
17
The axis is part of an active transform (TRUE state).
ControlledByTransformStatus
18
The axis is moving because of a transform (TRUE state).
DirectVelocityControlStatus
19
The axis is not under Direct Velocity Control (FALSE state).
DirectTorqueControlStatus
20
The axis is not under Direct Torque Control (FALSE state).
MoveLockStatus
22
MAM is Locked to Master in MDSC Mode (TRUE state).
The bit is cleared when a MGS, MGSD, MAS, or MASD is executed (goes IP).
If either the Slave or Master axis (or both) is paused by changing its speed to 0, then the MoveLockStatus bit stays set.
Master Driven Mode
The bit is set when the Lock Direction request is satisfied.
The bit is not used when the enumeration is NONE.
For the enumerations Immediate Forward Only and Immediate Reverse Only, the MamLockStatus bit is set immediately when the MAM is initiated.
For the enumeration Position Forward Only and Position Reverse Only, the bit is set when the Master Axis crosses the Master Lock Position in the specified direction.
The MoveLockStatus bit is cleared when the Master Axis reverses direction and the Slave Axis stops following the Master Axis. The MoveLockStatus bit is set again when the Slave Axis resumes following the Master Axis.
Time Driven Mode
The bit is not used when the enumeration is NONE.
JogLockStatus
24
The axis is not in a Jog Locked condition (FALSE state).
MasterOffsetMoveLockStatus
26
Master offset Move is Locked to master in MDSC Mode (TRUE state).
MaximumSpeedExceeded
27
Sets when the maximum axis speed that is specified in the axis configuration is exceeded during a move (TRUE state). Clears when the speed is reduced below the limit (FALSE state).
Motion Status Bits
If the Move Type Is
And Merge is
Then the Instruction Changes These Bits
Bit Name
State
Meaning
NOT Absolute Master Offset or Incremental Master Offset
Disabled
MoveStatus
TRUE
Axis is Moving.
Enabled
MoveStatus
TRUE
Axis is Moving.
JogStatus
FALSE
Axis is no longer Jogging.
GearingStatus
FALSE
Axis is no longer Gearing.
Absolute Master Offset or Incremental Master Offset
arrow_right (2)
MasterOffsetMoveStatus
TRUE
Axis is Offset.
Merging in Incremental Mode
The Merge for MAM operates differently from a merge on a Motion Coordinated Linear Move (MCLM) instruction. For the MAM, any uncompleted motion at the point of the merge remains in the move. For example, assume that you have a single axis MAM programmed in incremental mode from a starting absolute position = 0 and with the programmed incremental distance = 4 units. If a merge occurs at an absolute position of 1 and the merge is another incremental move of 4 units, the move completes at a position = 8.
If this example occurs on a Motion Coordinated Linear Move (MCLM) instruction programmed in incremental mode, the final position = 5.
Master Driven Speed Control (MDSC) Merging and Replacement Mode for MAM
When programmed in units of seconds, the MAM instruction must start at rest (that is, both start velocity and acceleration must be equal to 0.0). If programmed in units of seconds or Master Units, a runtime error will occur for the MAM on the Slave if the instruction is activated when not at rest.
Master Driven Speed Control (MDSC) and Motion Direct Command Support
The Motion Direct commands are not available in the instruction tree for the MDAC instruction. You must program an MDAC in one of the supported programming languages before you execute an MAM in Time Driven Mode. A runtime error will occur if an MDAC is not previously executed in an MAM or MAJ in Master Driven Mode.
The Motion Direct Command supports the MDSC enumerations speed, acceleration, deceleration, and Jerk for MAM.
Note that Event Distance and Calculated Data are not supported parameters for the MAM and Motion Direct Command.
Master Driven Speed Control (MDSC) and CIP Axis Manual Tune and Motion Generator
Event Distance and Calculated Data parameters are not supported for MAM.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal