Specify the Communication Details

Set up a broadcast in ladder logic or structured text programs. In ladder logic, add a rung and click on the
MSG
property to access the
Message Configuration
dialog box and set up a new message. In structured text, type
MSG
(aMsg ) and then right-click the aMsg to open the
Message Configuration
dialog box and configure the message.
NOTE: Logix Designer versions 37 and later do not support controllers with serial ports. The
Broadcast
button appears only in Logix Designer versions 36 and earlier for controllers with a serial port.
To configure a MSG instruction, specify the following on the
Communication
tab:
MSG_LD_Pg202_v31
Specify a Path
The path shows the route that the message takes to get to the destination. It uses names from the I/O configuration of the controller, numbers that you type, or both. You can default the path by using the broadcast button, which must be enabled with the system protocol and message type.
If
Then
The I/O configuration of the controller has the module that gets the message.
Browse to select the module.
The I/O configuration of the controller has only the local communication module.
Browse to select the local communication module and type the rest of the path.
The I/O configuration of the controller does not have any of the modules required for the message.
Type the path.
TIP:
Also supported is THIS, which indicates a path to self. THIS is used to send an unconnected message to the controller.
Examples
The I/O configuration of the controller has only the local communication module:
RSL5K_LocalCommModule
To type a path, use the format:
port, next_address, port, next_address,
Where
Is
For this network
Type
Port
Backplane
1
DF1 (serial, serial channel 0)
2
ControlNet
EtherNet/IP
DH+ channel A
DH+ channel B
3
DF1 channel 1 (serial channel 1)
Next_address
Backplane
Slot number of the module
DF1 (serial)
Station address (0-254)
ControlNet
Node number (1-99 decimal)
DH+
8# followed by the node number (1-77 octal)
For example, to specify the octal node address of 37, type 8#37.
EtherNet/IP
Specify a module on an EtherNet/IP network by using any of these formats:
  • IP address. For example, 10.10.10.10
  • IP address:Port. For example, 10.10.10.10:24
  • DNS name. For example, tanks
  • DNS name:Port. For example, tanks:24
Broadcast Button
The
Broadcast
button is used with the serial port.
  • This functionality for RSLogix 5000 software, beginning with version 18, enhances the ability to define the route and message type that are required to send a message to its destination.
The
Broadcast
button, when enabled, allows you to default the path by selecting an available channel(s) in a combo box. The number of channels listed in the combo box depends on the current controller.
By default, the
Path
button on the
Communication
tab is active.
Perform these steps to enable the
Broadcast
button and select a channel to default a path for the message.
  1. On the
    Controller Organizer
    , right-click
    Controller
    , and select
    Properties
    . The
    Controller Properties
    dialog box appears.
  2. Click the
    System Protocol
    tab.
  3. Select
    DF1 Master
    in the
    Protocol
    box. The Polling mode defaults ‘Message Based’ (slave can initiate messages).
  4. Click
    OK
    .
  5. In ladder logic, click the box inside the MSG tag. The
    Message Configuration
    dialog box appears with the
    Configuration
    tab open.
  6. In the
    Message Type
    box, select
    CIP Data Table Write
    .
  7. Click
    OK
    .You have enabled the
    Broadcast
    button on the
    Communication
    tab.
  8. Click the
    Communication
    tab.
  9. Next to the
    Broadcast
    button, select a channel in the combo box. The number of channels in the combo box depends on the controller.
    When you select channel 0 or 1, the corresponding message path on the
    Message Configuration
    dialog box defaults to 2,255 (channel 0) or 3,255 (channel 1). The Path grays out to not allow you to manually enter a path value.
  10. Click
    OK
    .
System Protocol Tab Configuration
NOTE: Logix Designer versions 37 and later do not support controllers with serial ports. The
System Protocol
tab appears only in Logix Designer versions 36 and earlier for controllers with a serial port.
To run broadcast in
ControlLogix
controllers in the Logix Designer application, you must configure the
System Protocol
tab in the
Controller Properties
dialog box. The protocol must be compatible with the message type of ‘write’ on the
Message Configuration
dialog box.
Follow these steps to set up the system protocol to be compatible with the broadcast feature.
  1. Create or open an existing controller in the application.
  2. On the
    Controller Organizer
    , right-click the controller name, and select
    Properties
    .The
    Controller Properties
    dialog box appears.
  3. If you controller has a serial port, click
    System Protocol
    tab.
    SystemProtocol_Pg205_v31
  4. In the Protocol box, select a protocol.
    IMPORTANT:
    The
    Message Type
    box on the
    Message Configuration Tab
    dialog box must be write-typed to be compatible with the system protocol. Otherwise, the
    Broadcast
    button is disabled.
  5. Enter the information on the
    System Protocol
    tab for each protocol outlined in the following tables.
    Topic
    Description
    Protocol
    DF-1 Master
    Station Address
    Type controller station address number
    Transmit Retries
    3
    ACK Timeout
    50
    Reply Message Wait
    5
    Polling Mode
    Select from the following modes:
    • Message Based
      Poll the slave using message instruction
    • Slave can initiate message
      for slave to slave broadcast
    • Standard
      . to have the schedule poll for the slave
    Error Detection
    BCC
    Duplicate Detection
    Enabled (checked)
    Topic
    Description
    Protocol
    DF-1 Slave
    Station Address
    Type controller station address number
    Transmit Retries
    3
    Slave Poll Timeout
    3000
    EOT Suppression
    Disable (unchecked)
    Error Detection
    BCC
    Duplicate Detection
    Enabled (checked)
    Topic
    Description
    Protocol
    DF-1 Slave
    Station Address
    Type controller station address number
    Enable Store and Forward
    Enable box (checkmark) to use store and forward tag
    Error Detection
    BCC
  6. Click
    OK
    .
For Block Transfers
For block transfer messages, add the following modules to the I/O configuration of the controller:
For block-transfers over this network:
Add these modules to the I/O configuration:
ControlNet
Local communication module (for example, 1756-CNB module)
Remote adapter module (for example, 1771-ACN module)
Universal remote I/O
Local communication module (for example, 1756-DHRIO module)
One remote adapter module (for example, 1771-ASB module) for each rack, or portion of a rack, in the chassis
Block-transfer module (optional)
Specify a Communication Method or Module Address
Use the following table to select a communication method or module address for the message:
If the destination device is
Select
And specify
Logix 5000
controller
CIP
No other specifications required.
PLC-5 controller over an EtherNet/IP network
PLC-5 controller over a ControlNet network
SLC 5/05 controller
PLC-5 controller over a DH+ network
DH+
Channel
Channel A or B of the 1756-DHRIO module that is connected to the DH+ network.
SLC controller over a DH+ network
Source Link
Link ID assigned to the backplane of the controller in the routing table of the 1756-DHRIO module. The source node in the routing table is automatically the slot number of the controller.
PLC-3 processor
Destination Link
Link ID of the remote DH+ link where the target device resides.
PLC-2 processor
Destination Node
Station address of the target device, in octal.
If there is only one DH+ link and you did not use the
RSLinx Classic
software to configure the DH/RIO module for remote links, specify 0 for both the Source Link and the Destination Link.
Application on a workstation that is receiving an unsolicited message routed over an EtherNet/IP or ControlNet network through
RSLinx Classic
or
FactoryTalk Linx
software
CIP with Source ID
This lets the application receive data from a controller.
Source Link
Remote ID of the topic in
RSLinx Classic
software, or the shortcut in
FactoryTalk Linx
.
Destination Link
Virtual Link ID set up in
RSLinx Classic
or
FactoryTalk Linx
software (0…65535).
Destination Node
Destination ID (0…77 octal) provided by the application to
RSLinx Classic
or
FactoryTalk Linx
. For a DDE topic in
RSLinx Classic
, use 77.
The slot number of the ControlLogix controller is used as the Source Node.
Block transfer module over a universal remote I/O network
RIO
Channel
Channel A or B of the 1756-DHRIO module that is connected to the RIO network.
Rack
Rack number (octal) of the module.
Group
Group number of the module.
Slot
Slot number of the module.
Block transfer module over a ControlNet network
ControlNet
Slot
Slot number of the module.
Choose a Cache Option
Depending on the configuration of an MSG instruction, it may use a connection to send or receive data.
Message type:
Communication method:
Uses a connection:
CIP data table read or write
Your option(1)
PLC-2, PLC-3, PLC-5, or SLC (all types)
CIP
CIP with Source ID
DH+
X
CIP generic
Your option(2)
Block-transfer read or write
X
  1. CIP data table read or write messages can be connected or unconnected. For most applications,
    Rockwell Automation
    recommends that you leave CIP data table read or write messages connected.
  2. CIP generic messages can be connected or unconnected. But, for most applications, we recommend you leave CIP generic messages unconnected.
If a MSG instruction uses a connection, you have the option to leave the connection open (cache) or close the connection when the message is done transmitting.
If you:
Then:
Cache the connection
The connection stays open after the MSG instruction is done. This optimizes execution time. Opening a connection each time the message executes increases execution time.
Do not cache the connection
The connection closes after the MSG instruction is done. This frees up that connection for other uses.
The controller has the following limits on the number of connections that you can cache.
If you have this controller:
Then you can cache:
CompactLogix
5370 or
ControlLogix
5570
Up to 32 connections.
ControlLogix
5580
Up to 256 connections.
If several messages go to the same device, the messages may be able to share a connection.
If the MSG instructions are to:
And they are:
Then:
Different devices
Each MSG instruction uses 1 connection.
Same device
Enabled at the same time
Each MSG instruction uses 1 connection.
NOT enabled at the same time
The MSG instruction uses 1 connection and 1 cached buffer. They share the connection and the buffer.
TIP:
To share a connection, if the controller alternates between sending a block-transfer read message and a block-transfer write message to the same module, both messages count as one connection. Caching both messages counts as one on the cache list.
Guidelines
As you plan and program your MSG instructions, follow these guidelines:
Guideline
Details
For each MSG instruction, create a control tag.
Each MSG instruction requires its own control tag.
Data type = MESSAGE
Scope = controller
The tag cannot be part of an array or a user-defined data type.
Keep the source and/or destination data at the controller scope.
A MSG instruction can access only tags that are in the Controller Tags folder (controller scope).
If your MSG is to a device that uses 16-bit integers, use a buffer of INTs in the MSG and DINTs throughout the project.
If your message is to a device that uses 16-bit integers, such as a PLC-5 or SLC 500 controller, and it transfers integers
(not REALs), use a buffer of INTs in the message and DINTs throughout the project.
This increases the efficiency of your project because Logix controllers execute more efficiently and use less memory when working with 32-bit integers (DINTs).
To convert between INTs and DINTs, see the Logix 5000 Controllers Common Procedures Programming Manual, publication 1756-PM001.
Cache the connected MSGs that execute most frequently.
Cache the connection for those MSG instructions that execute most frequently, up to the maximum number permissible for your controller revision.
This optimizes execution time because the controller does not have to open a connection each time the message executes.
For the
CompactLogix
5370 or
ControlLogix
5570 controllers , if you want to enable more than 16 MSGs at one time, use some type of management strategy.
For the
ControlLogix
5580 controllers, if you want to enable more than 256 MSGs at one time, use some type of management strategy.
For the
CompactLogix
5370 or
ControlLogix
5570 controllers, if you enable more than 16 MSGs at one time, some MSG instructions may experience delays in entering the queue.
For the
ControlLogix
5580 controllers, if you enable more than 256 MSGs at one time, some MSG instructions may experience delays in entering the queue.
To help make sure that each message executes, use one of these options:
Enable each message in sequence.
Enable the messages in groups.
Program a message to communicate with multiple devices. For more information, see the
Logix 5000
Controllers Common Procedures Programming Manual
, publication 1756-PM001.
Program logic to coordinate the execution of messages. For more information, see the
Logix 5000
Controllers Common Procedures Programming Manual
, publication 1756-PM001.
(For the
CompactLogix
5370 or
ControlLogix
5570 controllers only) Keep the number of unconnected and uncached MSGs less than the number of unconnected buffers.
The controller can have 10…40 unconnected buffers. The default number is 10 for the
CompactLogix
5370 or
ControlLogix
5570 controllers.
If all the unconnected buffers are in use when an instruction leaves the message queue, the instruction errors and does not transfer the data.
You can increase the number of unconnected buffers (40 max), but continue to follow guideline 5.
To increase the number of unconnected buffers, see the
Logix 5000
Controllers Common Procedures Programming Manual
, publication 1756-PM001.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal