MSG Configuration Examples

The following examples show source and destination tags and elements for different controller combinations.
The table explains the path for MSG instructions originating from a
Logix 5000
controller and being written to another controller.
Message Path
Example Source and Destination
Logix 5000
->
Logix 5000
Source tag
array_1[0]
Destination tag
array_2[0]
You can use an alias tag for the source tag in the originating
Logix 5000
controller.
You cannot use an alias for the destination tag. The destination must be a base tag.
Logix 5000
-> PLC-5
Logix 5000
-> SLC
Source tag
array_1[0]
Destination element
N7:10
You can use an alias tag for the source tag, in the originating
Logix 5000
controller.
Logix 5000
-> PLC-2
Source tag
array_1[0]
Destination element
010
The table explains the path for MSG instructions originating from a
Logix 5000
controller and reading from another controller.
Message Path
Example Source and Destination
Logix 5000
->
Logix 5000
Source tag
array_1[0]
Destination tag
array_2[0]
You cannot use an alias tag for the source tag. The source must be a base tag.
You can use an alias tag for the destination tag, in the originating
Logix 5000
controller.
Logix 5000
-> PLC-5
Logix 5000
-> SLC
Source element
N7:10
Destination tag
array_1[0]
You can use an alias tag for the destination tag, in the originating
Logix 5000
controller.
Logix 5000
-> PLC-2
Source element
010
Destination tag
array_1[0]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal