Access the TimeSynchronize object

The TIMESYNCHRONIZE object provides a Common Industrial Protocol (CIP) interface to the IEEE 1588 (IEC 61588) Standard for a precision clock synchronization protocol for networked measurement and control systems. Access the TIMESYNCHRONIZE object through the GSV/SSV instructions.
Attribute
Data Type
Instruction
Description
ClockType
INT
GSV
The type of clock.
Bit
Type of Clock
0
Ordinary Clock
1
Boundary Clock
2
Peer-to-peer transparent clock
3
End-to-end transparent clock
4
Management Node
All other bits are reserved.
CurrentTimeMicroseconds
DINT[2]
DT
LINT
GSV
Current value of System Time in microseconds.
CurrentTimeNanoseconds
LINT
LDT
GSV
Current value of System Time in nanoseconds.
DomainNumber
SINT
GSV
The PTP clock domain. The value is between 0...255. The default is 0.
CurrentTimeMicroseconds
LINT
DINT
GSV
Current value of System Time in microseconds.
CurrentTimeNanoseconds
LINT
LDT
GSV
Current value of System Time in nanoseconds.
DomainNumber
SINT
GSV
The PTP clock domain. The value is between 0...255. The default is 0.
GrandMasterClockInfo
Structure
GSV
Property information about the grandmaster clock.
Requires 24 bytes of storage.
Grandmaster Clock Information structure:
ClockIdentity
SINT[8]
ClockClass
INT
TimeAccuracy
INT
OffsetScaledLogVariance
INT
CurrentUtcOffset
INT
TimePropertyFlags
INT
TimeSource
INT
Priority1
INT
Priority2
INT
IsSynchronized
DINT
GSV
Local clock is synchronized with a master.
Value
Meaning
0
Not synchronized
1
Synchronized
LocalClockInfo
Structure
GSV
Property information about the local clock.
Requires 20 bytes of storage.
Local Clock Information structure:
ClockIdentity
SINT[8]
ClockClass
INT
TimeAccuracy
INT
OffsetScaledLogVariance
INT
CurrentUtcOffset
INT
TimePropertyFlags
INT
TimeSource
INT
ManufactureIdentity
DINT
GSV
The IEEE OUI (Organization Unique Identity) for the manufacturer.
MaxOffsetFromMaster
LINT
DINT
GSV / SSV
Maximum offset from master in nanoseconds.
MeanPathDelayToMaster
LINT
DINT
GSV
Average path delay from master to local clock in nanoseconds.
NumberOfPorts
INT
GSV
The number of ports of this clock.
OffsetFromMaster
LINT
DINT
GSV
The calculated difference between the local clock and the master clock, based on the most recent Sync message, in nanoseconds.
PTPEnable
DINT
GSV / SSV
The enable status for CIP Sync/PTP/Time Synchronization on the device.
Value
Meaning
0
Disable
1
Enable
ParentClockInfo
Structure
GSV
Property information about the parent clock.
Requires 16 bytes of storage.
Parent Clock Information structure:
ClockIdentity
SINT[8]
PortNumber
INT
ObservedOffsetScaledLogVariance
INT
ObservedPhaseChangeRate
DINT
PortEnableInfo
Structure
GSV
The port enable configuration of each port on the device.
Size = 2 + (No. of Enabled Ports x 4)
Maxsize = 42 bytes
Port Enable status structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
PortEnable
INT
PortLogAnnounceIntervalInfo
Structure
GSV
The interval between successive "Announce" messages issued by a master clock on each PTP port of the device.
Size = 2 + (No. of Enabled Ports x 4)
Maxsize = 42 bytes
Port Log Announce Interval structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
PortLogAnnounceInterval
INT
PortLogSyncIntervalInfo
Structure
GSV
The interval between successive Sync messages issued by a master on each PTP port of the device.
Size = 2 + (No. of Enabled Ports x 4)
Maxsize = 42 bytes
Port Log Sync Interval structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
PortLogAnnounceInterval
INT
PortPhysicalAddressInfo
Structure
GSV
The physical and protocol address of each port of the device.
Size = 2 + (No. of Enabled Ports x 36)
Maxsize = 362 byts
Port Physical Address structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
Protocol
SINT[16]
SizeOfAddress
INT
Port Address
SINT[16]
PortProfileIdentityInfo
Structure
GSV
Profile of each port of the device.
Size = 2 + (No. of Enabled Ports x 10)
Maxsize = 102
Port Profile Identity structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
ClockIdentity
SINT[8]
PortProtocolAddressInfo
Structure
GSV
The network and protocol address of each port of the device.
Size = 2 + (No. of Enabled Ports x 22)
Maxsize = 222
Port Protocol Address structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
NetworkProtocol
INT
SizeOfAddress
INT
PortAddress
SINT[16]
PortStateInfo
Structure
GSV
The current state of each PTP port on the device.
Size = 2 + (No. of Enabled Ports x 4)
Maxsize = 42 bytes
Port State structure:
NumberOfPorts
INT
Maximum number of ports is 10.
Structure repeated for the number of ports:
PortNumber
INT
PortState
INT
Priority1
SINT
GSV / SSV
Priority1 (Master Override) value for the local clock.
Note:
Value is Unsigned.
Priority2
SINT
GSV / SSV
Priority2 (Tie Breaker) value for the local clock.
Note:
Value is Unsigned.
ProductDescription
Structure
GSV
Product description of the device that contains the clock.
Requires 68 bytes of storage.
Product Description structure:
Size
DINT
Description
SINT[64]
RevisionData
Structure
GSV
Revision data of the device that contains the clock.
Requires 36 bytes of storage.
Revision Data structure:
Size
DINT
Revision
SINT[32]
StepsRemoved
INT
GSV
The number of CIP Sync Regions between the local clock and the grandmaster (that is, the number of boundary clocks +1)
SystemTimeAndOffset
Structure
GSV
System time in microseconds and the offset to the local clock value.
System Time and Offset structure:
SystemTime
LINT
DINT
SystemOffset
LINT
DINT
UserDescription
Structure
GSV
User description of the device that contains the clock.
Requires 132 bytes of storage.
User Description structure:
Size
DINT
Description
SINT[128]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal