Access the Program object

The Program object provides status information about a program. Specify the program name to determine the Program object you want.
Attribute
Data Type
Instruction within Standard Task
Instruction within Safety Task
Description
DisableFlag
SINT
GSV SSV
None
Controls this program’s execution. Each value has a specific meaning:
  • 0. Execution enabled.
  • Non zero. Execution disabled.
DINT
GSV
GSV
A non-zero value disables.
LastScanTime
DINT
TIME32
GSV SSV
None
Time to execute program the last time it was executed. Time is in microseconds.
MaxScanTime
DINT
TIME32
GSV SSV
None
Maximum recorded execution time for this program. Time is in microseconds.
MajorFault
Record
DINT[11]
GSV SSV
GSV SSV
Records major faults for this program.
MinorFault
Record
DINT[11]
GSV SSV
GSV SSV
Records minor faults for this program.
Name
String
GSV
GSV
Name of the program.
TIP:
Rockwell Automation recommends creating a user-defined structure to simplify access to either Fault Record attribute:
Name
Data Type
Style
Description
Timestamp
LINT
Decimal
The time at which the fault occurred. Units are microseconds since Jan 1, 1970.
Type
INT
Decimal
Fault type (program, I/O, and so forth)
Code
INT
Decimal
Unique code for the fault (depends on fault type)
Info
DINT[8]
Hexadecimal
Fault specific information (depends on fault type and code)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal