Access the AddOnInstructionDefinition Object

The
AddOnInstructionDefinition
object lets you customize instructions for sets of commonly-used logic, provides a common interface to this logic, and provides documentation for the instruction.
Attribute
Data Type
Instruction within Standard Task
Instruction within Safety Task
Description
LastEditDate
LINT
GSV
None
Timestamp of the last edit to an Add-On Instruction.
MajorRevision
DINT
GSV
None
Major revision number of the Add-On Instruction.
MinorRevision
DINT
GSV
None
Minor revision number of the Add-On Instruction.
Name
String
GSV
GSV
Name of the Add-On Instruction.
RevisionExtendedText
String
GSV
None
Text describing the revision of the Add-On Instruction.
SafetySignature
ID
DINT
GSV
None
In a safety project, the ID number, date, and timestamp of an Add-On Instruction definition.
SignatureID
DINT
GSV
None
32-bit identification number of an Add-On Instruction definition.
Vendor
String
GSV
None
Vendor that created the Add-On Instruction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal