Immediate values
    When you enter an immediate value (constant) in decimal format (for example, -2, 3) the controller stores the value by using 32 bits. If you enter a value in a radix other than decimal, such as binary or hexadecimal, and do not specify all 32 bits, the controller places a zero in the bits that you do not specify (zero-fill).
     IMPORTANT: 
    
Zero-fill of immediate binary, octal or hexadecimal values less than 32 bits.
| If you enter | The controller stores | 
| -1 | 16#ffff ffff (-1) | 
| 16#ffff (-1) | 16#0000 ffff (65535) | 
| 8#1234 (668) | 16#0000 029c (668) | 
| 2#1010 (10) | 16#0000 000a (10) | 
Integer Immediate Values
| If you enter | The controller stores | 
| Without any suffix | DINT | 
| "U" or "u" | UDINT | 
| "L" or "l" | LINT | 
| "UL", "ul", "Ul", or "uL" | ULINT | 
Floating Point Immediate Values
| If you enter | The controller stores | 
| Without any suffix | REAL | 
| "L" or "l" | LREAL | 
Provide Feedback