Result codes for SOVR instructions

When a tag is assigned to store the result of an
Equipment Sequence
Override (SOVR) instruction, the instruction returns one of these codes when it executes.
Code (Dec)
Description
0
The command was successful.
48
The command was not executed because it was not possible at the time to generate an event to record the command.
  • If the command was an ABORT command, the ABORT command is still executed even if the event could not be generated.
  • This code only occurs if event generation has been enabled in the
    Equipment Sequence Properties - Configuration
    tab.
24577
The command is not valid.
24578
The command is not valid for the current state of the
Equipment Sequence
. For example, if the
Equipment Sequence
is stopped, then a stop command is not valid.
24594
The
Equipment Sequence
is unscheduled, inhibited, or in a task that is inhibited.
Use the
Result
operand to get a code that shows the success or failure of the SOVR instruction. The
Result
operand should contain either
0
or a DINT tag, depending on whether ownership conflicts or other errors are likely to occur.
  • If ownership conflicts or other errors are not likely, enter
    0
    in the
    Result
    operand.
  • If ownership conflicts or other errors are likely, enter a DINT tag in the
    Result
    operand. The DINT tag stores a code for the result of the execution of the instruction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal