Jerk Rate Calculation

If the instruction uses or changes an S-curve profile, the controller calculates acceleration, deceleration, and jerk when you start the instruction.
Jerk is calculated as follows:
  • Accel Jerk = (Max Accel
    2
    / Max Velocity) * (200 / % of Time - 1)
  • Decel Jerk = (Max Decel
    2
    / Max Velocity) * (200 / % of Time - 1)
Which revision do you have?
  • 15 or earlier – % of Time is fixed at 100.
  • 16 or later – % of Time defaults to 100, but you can change it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal