Saving ACD File vs Upload of Project

The following is an example of a sequence of events that can generate an APR fault.
  1. Make an online change to an axis attribute that generates an APR fault.
  2. Rehome the axis.
    This is normally done so APR will restore axes positions after a download.
  3. Save your project.
  4. Download your project.
An APR fault occurs because saving the project only uploads the tags, not the changed attributes.
NOTE:
Upload the project to save the changed attributes and prevent an APR fault on a subsequent download.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal