Reset an APR Fault

There are three ways to reset an APR Fault.
  • Instruction Execution
    Executing an MAFR
    Executing an MGSR
    Executing an MASR
    Executing an MCSR
  • From the Controller Organizer:
    Clear the group fault, the
    Logix Designer
    application executes an MGSR
    Clear the axis fault, the application executes an MASR
  • Downloading the same project a second time
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal