Local Mode Configuration Attribute

This is the local mode attribute associated with a Motion Control Axis. This attribute governs the behavior of the Motion Control Axis when a local drive, for example, a non-CIP Motion, device interface requests control of axis behavior.
Local Control
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - All
Set
USINT
0
-
-
Enumeration
0 = Not Allowed (R)
1 = Conditionally Allowed (O)
2 = Allowed (O)
3...255 = Reserved
Mechanism for controller to allow a local interface to request local control. Control implies in this case the ability to change the state or behavior of the axis. Possible values:
  • Not Allowed (0) - Configures the device to prevent a local interface from taking control of the drive.
  • Conditionally Allowed (1) - Configures the device to prevent a local interface from taking control of the axis while the axis is in an Operational State, such as Running or Testing.
  • Allowed (2) - Configures the device to allow a local interface to take control of the axis, even in an Operational State. Some devices may not support this state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal