Guard Safety Attributes

These are the attributes associated with the built-in Safety functionality of an axis. These attributes relate to the behavior of a configurable Safety Core within the drive that executes basic drive safety functions using hardwired safety inputs and safety outputs. These functions do not require the services of a CIP Safety network connection. This safety functionality covers the following safety functions as defined by IEC-61800-5-2, EN-954-1, and IEC-60204 standards:
  • Safe Restart
  • Safe Stop
  • Safe Limited Speed
  • Safe Speed Monitoring
  • Safe Maximum Speed
  • Safe Direction Monitoring
  • Safe Door Monitoring
  • Safe Door Monitoring
The Guard Status and Guard Fault attributes are defined in the axis to monitor the behavior of built-in Drive Safety functionality. The term Guard is used for these status attributes to differentiate these attributes from the Safety status attributes associated with the integrated Safety functionality provided by a CIP Safety connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal