Drive Parameters

When getting a drive attribute value, you must configure the system to cyclically update these attributes. Using just a GSV or Axis tag without configuring the system in this way will not get the current attribute value in the drive.
Setting the drive attribute can, however, be done directly with a SSV instruction. Changes to an Axis Tag value will not update the drive parameter without first configuring the system to cyclically update these drive parameters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal