Command Ref Generation Attributes

These are the command reference generation functionality of the device that converts command position, velocity, acceleration, and torque data output from a controller-based or device-based motion planner into corresponding command references signals to the device's motor control structures. The command reference generator functionality includes fine interpolators, signal selector switches, dynamic limiters, command notch filters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal