CAM_EXTENDED Structure

The CAM_EXTENDED data type consists of slave and master point pairs, as well as an interpolation type. Because there is no association with a specific axis position or time, the point values are unitless. You can specify the interpolation type for each segment as either linear or cubic. CAM_EXTENDED is supported by
Compact GuardLogix
5580,
CompactLogix
5380, and
CompactLogix
5480 controllers only.
This table describes the format of the cam array element:
Mnemonic
Data Type
Description
MASTER
LREAL
The x value of the point.
SLAVE
LREAL
The y value of the point.
Segment Type
DINT
The type of interpolation
0 = linear
1 = cubic
TIP:
You cannot convert the CAM data type to CAM_EXTENDED, and you cannot convert the CAM_EXTENDED data type to CAM.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal