CAM Structure

The CAM data type consists of slave and master point pairs, as well as an interpolation type. Because there is no association with a specific axis position or time, the point values are unitless. Specify the interpolation type for each segment as either linear or cubic. This table describes the format of the cam array element:
Mnemonic
Data Type
Description
MASTER
REAL
The x value of the point.
SLAVE
REAL
The y value of the point.
Segment Type
DINT
The type of interpolation
0 = linear
1 = cubic
TIP:
You cannot convert the CAM data type to CAM_EXTENDED, and you cannot convert the CAM_EXTENDED data type to CAM.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal