Digital Alarm (ALMD)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers. Controller differences are noted where applicable.
The Digital Alarm (ALMD) instruction provides alarming for any discrete Boolean value.
Available Languages
Ladder Diagram
Function Block
Structured Text
ALMD (ALMD,In,ProgAck,ProgReset,ProgDisable,ProgEnable)
Operands
Ladder Diagram
Operand
Type
Format
Description
ALMD tag
ALARM_DIGITAL
Structure
ALMD structure
ProgAck
BOOL
Tag
Immediate
On transition from false to true, acknowledges alarm (if acknowledgment is required).
ProgReset
BOOL
Tag
Immediate
On transition from false to true, resets alarm (if resetting is required).
ProgDisable
BOOL
Tag
Immediate
When True, disables alarm (does not override Enable Commands).
ProgEnable
BOOL
Tag
Immediate
When True, enables alarm (takes precedence over Disable commands).
MinDurationPRE
DINT
Immediate
Specifies how long the alarm condition must be met before it is reported (milliseconds).
MinDurationACC
DINT
Immediate
Indicates the current accumulator value for the alarm’s MinDuration timer. This value is not used in versions 29 and later of the Logix Designer application. The value is always 0.
Function Block
Operand
Type
Format
Description
ALMD tag
ALARM_DIGITAL
structure
ALMD structure
Structured Text
Operand
Type
Format
Description
ALMD tag
ALARM_DIGITAL
Structure
ALMD structure
ProgAck
BOOL
Tag
Immediate
On transition from false to true, acknowledges alarm (if acknowledgment is required).
ProgReset
BOOL
Tag
Immediate
On transition from false to true, resets alarm (if resetting is required).
ProgDisable
BOOL
Tag
Immediate
When True, disables alarm (does not override Enable Commands).
ProgEnable
BOOL
Tag
Immediate
When True, enables alarm (takes precedence over Disable commands).
MinDurationPRE
DINT
Immediate
Specifies how long the alarm condition must be met before it is reported (milliseconds).
MinDurationACC
DINT
Immediate
Indicates the current accumulator value for the alarm’s MinDuration timer. This value is not used in versions 29 and later of the Logix Designer application. The value is always 0.
See Structured Text Syntax for more information on the syntax of expressions within structured text.
ALMD Structure
Input Parameters
Input Parameter
Data Type
Description
EnableIn
BOOL
Ladder Diagram:
Corresponds to the rung state. Does not affect processing.
Function Block:
If cleared to false, the instruction does not execute and outputs are not updated.
If set, the instruction executes.
Default is true.
Structured Text:
No effect. The instruction always executes.
In
BOOL
The digital signal input to the instruction.
Default is false.
Ladder Diagram:
Follows the rung condition. Set to true if the rung condition is true. Cleared to false if the rung condition is false.
Structured Text:
Copied from instruction operand.
InFault
BOOL
Bad health indicator for the input. The user application may set InFault to indicate the input signal has an error. When set, the instruction sets InFaulted (Status.1). When cleared to false, the instruction clears the InFaulted (Status.1) to false. In either case, the instruction continues to evaluate In for alarm conditions.
Default is false (good health).
Condition
BOOL
Specifies how alarm is activated. When Condition is set to true, the alarm condition is activated when In is set to true. When Condition is cleared to false, the alarm condition is activated when In is Cleared to false.
Default is true.
AckRequired
BOOL
Specifies whether alarm acknowledgment is required. When set to true, acknowledgment is required. When cleared to false, acknowledgment is not required and Acked is always set to true.
Default is true.
Latched
BOOL
Specifies whether the alarm is latched. Latched alarms remain InAlarm when the alarm condition becomes false, until a Reset command is received. When set to true, the alarm is latched. When cleared to false, the alarm is unlatched.
Default is false.
A latched alarm can only be reset when the alarm condition is false.
ProgAck
BOOL
Set to true by the user program to acknowledge the alarm. Takes effect only if the alarm is unacknowledged. Requires a false-to-true transition.
Default is false.
Ladder Diagram:
Copied from the instruction operand.
Structured Text:
Copied from the instruction operand.
OperAck
BOOL
Set to true by the operator interface to acknowledge the alarm. Takes effect only if the alarm is unacknowledged. The instruction clears this parameter.
Default is false.
ProgReset
BOOL
Set to true by the user program to reset the latched alarm. Takes effect only if the latched alarm is InAlarm and the alarm condition is false. Requires a false-to-true transition.
Default is false.
Ladder Diagram:
Copied from the instruction operand.
Structured Text:
Copied from the instruction operand.
OperReset
BOOL
Set to true by the operator interface to reset the latched alarm. Takes effect only if the latched alarm is InAlarm and the alarm condition is false. The alarm instruction clears this parameter to false.
Default is false.
ProgSuppress
BOOL
Set to true by the user program to suppress the alarm.
Default is false.
OperSuppress
BOOL
Set to true by the operator interface to suppress the alarm. The alarm instruction clears this parameter to false.
Default is false.
ProgUnsuppress
BOOL
Set to true by the user program to unsuppress the alarm. Takes precedence over Suppress commands.
Default is false.
OperUnsuppress
BOOL
Set to true by the operator interface to unsuppress the alarm. Takes precedence over Suppress commands. The alarm instruction clears this parameter to false.
Default is false.
OperShelve
BOOL
Set to true by the operator interface to shelve or reshelve the alarm. Requires a transition from false in one program scan to true in the next program scan. The alarm instruction clears this parameter to false.
Default is false.
Unshelve commands take precedence over Shelve commands.
Shelving an alarm postpones alarm processing. It is like suppressing an alarm, except that shelving is time limited. If an alarm is acknowledged while it is shelved, it remains acknowledged even if it becomes active again. It becomes unacknowledged when the shelve duration ends provided the alarm is still active at that moment.
ProgUnshelve
BOOL
Set to true by the user program to unshelve the alarm. Takes precedence over Shelve commands.
Default is false.
For more information on shelving an alarm, see the description for the OperShelve parameter.
OperUnshelve
BOOL
Set to true by the operator interface to unshelve the alarm. The alarm instruction clears this parameter to false. Takes precedence over Shelve commands.
Default is cleared.
For more information on shelving an alarm, see the description for the OperShelve parameter.
ProgDisable
BOOL
Set to true by the user program to disable the alarm.
Default is false.
Ladder Diagram:
Copied from the instruction operand.
Structured Text:
Copied from the instruction operand.
OperDisable
BOOL
Set to true by the operator interface to disable the alarm. The alarm instruction clears this parameter to true.
Default is false.
ProgEnable
BOOL
Set to true by the user program to enable the alarm. Takes precedence over a Disable command.
Default is false.
Ladder Diagram:
Copied from the instruction operand.
Structured Text:
Copied from the instruction operand.
OperEnable
BOOL
Set to true by the operator interface to enable the alarm. Takes precedence over Disable command. The alarm instruction clears this parameter to false.
Default is false.
AlarmCountReset
BOOL
Set to true by the operator interface to reset the alarm count to zero. The alarm instruction clears this parameter to false.
Default is false.
UseProgTime
BOOL
Specifies whether to use the controller’s clock or the ProgTime value to timestamp alarm state change events. When set to true, the ProgTime value provides timestamp. When cleared to false, the controller’s clock provides timestamp.
Default is false.
ProgTime
LINT
If UseProgTime is set to true, this value is used to provide the timestamp value for all events. This lets the application apply timestamps obtained from the alarm source, such as a sequence-of-events input module.
Severity
DINT
Severity of the alarm. This does not affect processing of alarms by the controller, but can be used for sorting and filtering functions at the alarm subscriber.
Valid = 1...1000 (1000 = most severe; 1 = least severe).
Default = 500.
MinDurationPRE
DINT
Minimum duration preset (milliseconds) for the alarm condition to remain true before the alarm is marked as InAlarm and alarm notification is sent to clients. The controller collects alarm data as soon as the alarm condition is detected; so no data is lost while waiting to meet the minimum duration.
Valid = 0...2147483647.
Default = 0.
ShelveDuration
DINT
Length of time in minutes to shelve an alarm. Shelving an alarm postpones alarm processing. It is like suppressing an alarm, except that shelving is time limited. If an alarm is acknowledged while it is shelved, it remains acknowledged even if it becomes active again. It becomes unacknowledged when the shelve duration ends (provided the alarm is still active at that time).
Minimum time is one minute. Maximum time is defined by MaxShelveDuration.
MaxShelveDuration
DINT
Maximum time duration in minutes for which an alarm can be shelved. For more information on shelving an alarm, see the description for the ShelveDuration parameter.
Output Parameters
Output Parameter
Data
Type
Description
EnableOut
BOOL
Enable output.
InAlarm
BOOL
Alarm active status. Set to true when the alarm is active. Cleared to false when the alarm is not active (normal status).
Acked
BOOL
Alarm acknowledged status. Set to true when the alarm is acknowledged. Cleared to false when the alarm is not acknowledged.
Acked is always set to true when AckRequired is cleared to false.
InAlarmUnack
BOOL
Combined alarm active and acknowledged status. Set to true when the alarm is active (InAlarm is true) and unacknowledged (Acked is false). Cleared to false when the alarm is inactive, acknowledged, or both.
Suppressed
BOOL
Suppressed status of the alarm. Set to true when the alarm is suppressed. Cleared to falsewhen the alarm is not suppressed.
Shelved
BOOL
Shelved status of the alarm. Set to true when alarm is shelved. Cleared to false when alarm is unshelved.
Shelving an alarm postpones alarm processing. It is like suppressing an alarm, except that shelving is time limited. If an alarm is acknowledged while it is shelved, it remains acknowledged even if it becomes active again. It becomes unacknowledged when the shelve duration ends.
Disabled
BOOL
Disabled status of the alarm. Set to true when the alarm is not enabled. Cleared to false when the alarm is enabled.
Commissioned
BOOL
Commissioned status of the alarm. Set to true when the alarm is commissioned. Cleared to false when the alarm is decommissioned. Currently always set to true.
MinDurationACC
DINT
Indicates the current accumulator value for the alarm’s MinDuration timer. This value is not used in versions 29 and later of the Logix Designer application. The value is always 0.
AlarmCount
DINT
Number of times the alarm has been activated (InAlarm is set). If the maximum value is reached, the counter leaves the value at the maximum count value.
InAlarmTime
LINT
Timestamp of alarm detection.
AckTime
LINT
Timestamp of alarm acknowledgment. If the alarm does not require acknowledgment, this timestamp is equal to alarm time.
RetToNormalTime
LINT
Timestamp of alarm returning to a normal state.
AlarmCountResetTime
LINT
Timestamp indicating when the alarm count was reset.
ShelveTime
LINT
Timestamp indicating when the alarm was shelved the last time. This value is set by controller when alarm is shelved. Alarm can be shelved and unshelved many times. Each time the alarm is shelved, the timestamp is set to the current time.
For more information on shelving an alarm, see the description for the Shelved parameter.
UnshelveTime
LIN
Timestamp indicating when the alarm is going to be unshelved. This value is set every time the alarm is shelved (even if the alarm has already been shelved). The timestamp is determined by adding the ShelveDuration to the current time. If the alarm is unshelved programmatically or by an operator, then the value is set to the current time.
For more information on shelving an alarm see the description for the Shelved parameter.
Status
DINT
Combined status indicators:
Status.0 = InstructFault
Status.1= InFaulted
Status.2 = SeverityInv
InstructFault (Status.0)
BOOL
Instruction error conditions exist. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
InFaulted
(Status.1)
BOOL
User program has set InFault to indicate bad quality input data. Alarm continues to evaluate In for alarm condition.
SeverityInv
(Status.2)
BOOL
Alarm severity configuration.
If severity <1, the instruction uses Severity = 1.
If severity >1000, the instruction uses Severity = 1000.
Digital Alarms State Diagrams
Digital Alarm Timing Diagrams
ALMD Alarm Acknowledge Required and Latched
ALMD Alarm Acknowledge Required and Not Latched
ALMD Alarm Acknowledge Not Required and Latched
ALMD Alarm Acknowledge Not Required and Not Latched
Connect a button to the OperShelve tag
To prevent unwanted reshelving of the alarm, the alarm instruction only processes the OperShelve tag if it transitions from false to true between one program scan and the next. If an operator presses a push button to shelve the alarm while the ProgUnshelve tag is true, the alarm is not shelved because the ProgUnshelve tag takes precedence. However, because program scans complete in milliseconds, the operator may still be holding down the push button so that the OperShelve tag remains true over several program scans even though the ProgUnshelve tag has been cleared to false. This means that the alarm is not shelved.
To shelve the alarm, the operator can release and press the button again
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
EnableOut is cleared to false to false
The InAlarm output is cleared to false
The Shelved output is cleared to false
The Acked ouput is set to true.
All alarm conditions are acknowledged.
All operator requests are cleared
All timestamps are cleared
Rung-condition-in is false
Rung is cleared to false.
The In parameter is cleared to false
The instruction executes.
Rung-condition-in is true
Rung is set to true.
The In parameter is set to true
The instruction executes.
Postscan
Rung bit is cleared to false.
Function Block
Condition/State
Action Taken
Prescan
Tag.EnableOut is cleared to false.
The InAlarm output is cleared to false
The Shelved output is cleared to false
The Acked ouput is set to true
All operator requests are cleared
All timestamps are cleared
Tag.EnableIn is false
Tag.EnableOut is cleared to false
Tag.EnableIn is true
The instruction executes
Tag.EnableOut is set to true
Instruction first run
N/A
Instruction first scan
N/A
Postscan
Tag.EnableOut is cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Normal Execution
See Rung-condition-in is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Example
Ladder Diagram
Function Block
Structured Text
An example of an ALMD instruction in Structured Text is shown below. In this example, two motor failure signals are combined such that if either one occurs, a motor fault alarm is activated. The Motor101Ack tag can be used to acknowledge the alarm.
Motor101FaultConditions := Motor101Overtemp OR Motor101FailToStart;
ALMD(Motor101Fault,Motor101FaultConditions,Motor101Ack,0,0,0 );
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal