Upgrade Multiple Projects

After uploading your projects to the FactoryTalk Vault, you can upgrade them to different Logix versions and different controller types.
  1. From the vault navigation pane, select the solution.
  2. From the project list, select the checkboxes for the projects you want to upgrade.
  3. From the vault toolbar, select
    Upgrade
    .
  4. From the
    Upgrade Logix Project
    page in the
    Select Logix Version
    pull-down list, choose the version of Logix controller to upgrade to.
  5. Select the checkboxes for the projects to upgrade.
  6. (optional) In the
    Select Controller Type
    pull-down list choose the controller catalog number to upgrade the project to.
  7. Review Warnings
    displays the impact of the upgrade of the project. Review the warning carefully.
    • Select
      Upgrade
      to continue with the upgrade process.
    • Select
      Cancel
      to stop the upgrade process.
The status of the projects changes to
Upgrading
. Notification messages appear to inform you of the upgrade process. Once the upgrade has completed, the project status changes to
Ready
if the project upgraded successfully. If problems were encountered in the upgrade, the status changes to
Error
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal