Delete a Project or Solution

Delete a project or solution when it is no longer needed.
  1. From the vault, select the checkbox for the project or solution. You can select multiple projects.
  2. From the vault toolbar, select
    Delete
    .
  3. When prompted, click
    Confirm
    to proceed with deleting the project or solution.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal