Routines Analysis Details

The
Routines
analysis dashboard displays the routines scheduled in the different programs of your project.
The
Routines
analysis dashboard details the number of routines per program in your project:
The dashboard displays the name of the program or equipment phase, the routine name, and the size of the program. It also identifies whether the routine is source-protected.
You can sort and filter the data in this dashboard. If you want to see the information in a different order, you can reorder the columns in the data table by dragging and dropping them as needed. To help you move around the analysis details page quickly, use keyboard shortcuts.
Routine Visualization
When you select a Logix Designer project in Vault you can view routines directly.
  1. In Vault select the Logix Designer project in which you want to view routines.
  2. Click Analysis in the top menu bar.
  3. Scroll down to the Routine Summary panel and click Details.
  4. On the Routine screen which appears, select Logic.
  5. Choose the routine you want to view. You can expand or collapse portions of the tree by clicking the arrow next to the selection. When you click the routine name you load a visual representation of the routine on the right side panel in either ladder logic, sequential block charts, functional block diagrams, or structured text. Use Ctrl + scroll to zoom in and out of the routine in Windows, or by using Cmd + scroll on MacOS.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal