Hardware Analysis Details

The
Hardware
analysis dashboard provides an overview of the hardware configuration in the project.
The hardware components list includes the following information:
  • Catalog Number — The Rockwell Automation catalog number of the hardware component
  • Description — The name of the hardware component
  • Revision — The firmware associated with the hardware component
  • Vendor — The original equipment manufacturer of the hardware components
  • Quantity — A count of the number of these hardware components identified in the project
You can sort and filter the data in this dashboard. If you want to see the information in a different order, you can reorder the columns in the data table by dragging and dropping them as needed. To help you move around the analysis details page quickly, use keyboard shortcuts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal