Log

The
FactoryTalk® Remote Access
Manager
contains a real-time log of domain-related activities. In this log you can find detailed information, such as:
  • The browser used to open a session through the
    FactoryTalk® Remote Access
    Manager
    .
  • Time and date connection to the remote Access Server.
  • Time and date when the server validated the access request.
  • Transaction start.
  • Amount of packet loss, latency, and jitter in the network communications.
  • Time and date of the transaction completion.
  • Time and date of a successful authentication.
  • Time and date of a failed authentication.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal