OptixPanel
Graphic Terminals

OptixPanel
Graphic Terminals integrate both FactoryTalk Optix and FactoryTalk Remote Access Runtime. Terminals are available in two configurations:
  • OptixPanel
    Standard Graphic Terminal
    : It is provided with a Runtime Pro entitlement.
  • OptixPanel
    Compact Graphic Terminal
    : It is provided with a Runtime Basic entitlement and allows to purchase an entitlement upgrade.
NOTE: See Entitlements for more information about this subject.
NOTE: For further information on the
OptixPanel
Graphic Terminals, see the documentation provided at the link OptixPanel Graphic Terminals.
NOTE: To learn more about the device System Manager, download this user manual:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal