Runtime container exposed ports
The Runtime container consistently exposes specific ports for various functionalities.
The Runtime container consistently exposes port 5161 for the Web UI, mapped to 127.0.0.1:5161
on the host. To access the Web UI, open your browser and navigate to https://localhost:5161.
Additionally, the Runtime container exposes port 5936 for local connections, which is directly mapped to port 5936 on the host.
Provide Feedback