Connection between FactoryTalk®
Remote Access™ Manager and remote devices
FactoryTalk®
Remote Access™
ManagerThe connection logic between the and a remote device occurs as
described below:
FactoryTalk®
Remote Access™
Manager- Theconnects to the Server Infrastructure and obtains a list of the devices registered to the user's domain.FactoryTalk® Remote Access™ManagerNOTE: See FactoryTalk Remote Access Manager overview and related entities for further information on domains.NOTE: The user owns the access permissions for the aforementioned devices. See Domain user permissions for further information on this subject.
- When you connect the remote device to the Server Infrastructure, thereceives a notification about this connection.FactoryTalk® Remote Access™ManagerNOTE: See (Interactive Access) Connection for further information on this topic.
- You can establish a VPN connection troughand access theFactoryTalk® Remote Access™ManagerRemote desktopservice.NOTE: See (Interactive Access) Remote desktop for further information on this topic.
Provide Feedback