Runtime connection lost

If the Tools lose the connection with the Runtime and the Runtime device is online, a blank page appears that says
Device disconnected
.
If the Tools lose the connection with the Runtime and the Runtime device is offline, the message says
Device offline
.
To re-establish a connection, select the
Reconnect
button that appears below the
Device disconnected
message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal