Enable FactoryTalk Remote Access for FactoryTalk Design Studio

You can configure communication between FactoryTalk Remote Access and FactoryTalk Design Studio by creating and configuring the FactoryTalk Remote Access
FTDS
user.
NOTE: To work together, the instances of FactoryTalk Remote Access and FactoryTalk Design Studio you are using must be entitled within the same organization in FactoryTalk Hub. FactoryTalk Design Studio can only communicate with the FactoryTalk Remote Access instance in the same FactoryTalk Hub organization. See Entitlements in the FactoryTalk Remote Access Online Help
This task requires you to have entitlements allocated for using FactoryTalk Remote Access.
  1. To enable the FTDS user in FactoryTalk Remote Access for use with FactoryTalk Design Studio:
  2. Open the FactoryTalk Remote Access application in FactoryTalk Hub.
  3. On the left side of the screen expand
    Settings
    by selecting the down arrow.
  4. Select
    Domain Options
    , the
    Options
    screen appears.
  5. Select the
    Enable FactoryTalk Design Studio (Linx) integration
    box and select
    Save
    .
    Selecting this option creates a FactoryTalk Remote Access user labeled
    FTDS
    which you will use to set permissions.
  6. Select
    Explorer > Domain View
    on the left side of the screen.
  7. Select the device or folder with the endpoints that you want to connect via FactoryTalk Design Studio. You can connect to a single endpoint or set permissions for all the endpoints you have placed in a folder for your organization.
    FactoryTalk Remote Access endpoint devices enable secure connectivity to your controllers. Granting endpoint access to the FTDS user enables FactoryTalk Design Studio to communicate through the endpoint to on-premises controllers. To deploy to an on-premise controller with FactoryTalk Design Studio, the controller must be accessible on the same network as a FactoryTalk Remote Access endpoint device.
    For more information on how to add an endpoint device, see:
    FactoryTalk Remote Access Manager Tools
    in the FactoryTalk Remote Access Help. For this step look at the help for
    Device Registration to Domain
    .
  8. Select the endpoint to which you want to assign permissions for the enabled
    FTDS
    user. An information panel opens on the right side of the screen.
  9. Select the arrow next to
    Permissions
    to expand the permissions list.
  10. Select the plus sign next to
    Permissions
    to add the FactoryTalk Design Studio user.
  11. Select the plus sign next to the user labeled
    FTDS
    to add the user then close the
    Add Permissions
    dialog by selecting the x at the top right of the box. The
    FTDS
    user now appears in the Permissions list.
  12. Select the
    FTDS
    user.
  13. Under
    Permissions Operations
    select the arrow to expand
    Interactive Access
    .
  14. Select the
    Allow
    box next to
    Network Access (VPN)
    . The
    FTDS
    user now has permission to access the selected endpoint device. To give the
    FTDS
    user permission to all endpoint devices in the organization, highlight the top level in your folder structure and repeat this process
FactoryTalk Design Studio can now use the
FTDS
user to communicate with devices connected to FactoryTalk Remote Access endpoints. Next you must configure the endpoints in FactoryTalk Design Studio. Go to Connect FactoryTalk Design Studio to FactoryTalk Remote Access
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal