Subdevices
Subdevices may consist of devices such as PLCs, drives, iPCs, and similar, that are connected to a subnetwork and operate in conjunction with a remote device such as a Runtime, a router, or an HMI.
You can add one or more subdevices for each remote device through the , and set any services for each
subdevice. In this way, you can directly connect to the subdevice services without having to
establish a VPN connection with the remote device first. When a connection establishes, an
application opens based on the subdevice IP address.
Domain
view
section in FactoryTalk®
Remote Access™
ManagerProvide Feedback