Groups creation

Groups consist of users collections and help organize users permissions. To create a group, log on to the
FactoryTalk® Remote Access
Manager
as an administrator user.
To create a users group, proceed as follows:
  1. Access the
    FactoryTalk® Remote Access
    Manager
    and select
    Explorer
    Domain view
    .
  2. Select the domain folder first and then select the
    Add resource
    (
    circled plus
    icon) nearby.
  3. Select
    Create group
    .
  4. Enter a group name.
  5. On the right pane, select the
    Add resource
    (
    circled plus
    icon) and search for existing user accounts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal