Approve remote access
The
Approve remote access
entry introduces an additional level of security on the remote device. It allows you to access the remote desktop or open a VPN channel only upon permission of the user, or by having direct access to the remote device. You can apply this setting to single devices only.
NOTE:
Device installer permissions are required to enable or disable the
Approve remote access
entry.To enable the
Approve remote access
feature on a remote device:
- Access theand select .FactoryTalk® Remote Access™Manager
- Select the remote device for which you would like to set theApprove remote accesspermission.
- On the right pane, flag theApprove remote accessoption.
When , an authorization window appears on
the remote device showing the username and IP address of the incoming user connection. The
operator of the remote device can then allow or deny access to the device. If access is
denied, a notification will inform you that the connection request was not allowed.
Approve remote access
is enabled on a device, and you attempt to
start a VPN connection or a remote desktop session through the FactoryTalk®
Remote Access™
ManagerProvide Feedback