Log in to FactoryTalk®
Hub™
FactoryTalk®
Hub™
FactoryTalk®
Hub™
includes different cloud-based SaaS applications, displayed in
the form of tiles. Log in to FactoryTalk®
Hub™
to access your application.- Go to FactorytalkHub.com to launchFactoryTalk® Hub™.
- TIP: If you do not have a MyRockwellAutomation account, see Create your MyRockwellAutomation account.In theSign inpane, enter the same email that you use for your MyRockwellAutomation account.
- Enter the same password that you use for your MyRockwellAutomation account.AImportant: MFA Skip Limit Warningmessage appears.
- In theSelect verification methodpane, select a verification option, and then selectCONTINUE.IMPORTANT: You can select a verification method other than email, such as SMS text message, or phone call. To select SMS text message or phone call, you must have entered your phone number when you created your MyRockwellAutomation account in theAdvanced Accesssection.
- Enter a verification code as required in theTwo-step verificationpane or enter the code on the phone, depending on the verification method that you previously selected.
- The first time you log in toFactoryTalk® Hub™, scroll to read the Rockwell Automation EULA and then selectAccept.You are prompted to either join an existing organization or create a new one.
TIP:
To learn more about the
FactoryTalk®
Hub™
, see FactoryTalk Hub online Help. Provide Feedback